# SPI between MSP430/432 and MCP3911

**URL:** <https://community.sparkfun.com/t/spi-between-msp430-432-and-mcp3911/33661>\
**Category:** MicroMod\
**Tags:** arm-lpc\
**Created:** [December 7, 2016, 10:34pm UTC](https://community.sparkfun.com/t/spi-between-msp430-432-and-mcp3911/33661 "2016-12-07T22:34:41Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![janak](https://avatars.discourse-cdn.com/v4/letter/j/65b543/32.png) [@janak](https://community.sparkfun.com/u/janak)\
**Post date:** [December 7, 2016, 10:34pm UTC](https://community.sparkfun.com/t/spi-between-msp430-432-and-mcp3911/33661/1 "2016-12-07T22:34:41Z")

</div>

Hi,

I am trying to read ADC channel values from MCP3911 using MSP launchpad using SPI protocol. When i used Arduino Mega the protocol is working fine. But when i use any TI devices i am having a problem, it always gives me all 0’S or 1’s.

I am using energia for MSP devices. Any i have chosen the appropriate pins as defined in the enegia pin layout.

static const uint8\_t SS = 8; /\* P2.7 \*/

static const uint8\_t SCK = 7; /\* P3.2 \*/

static const uint8\_t MOSI = 15; /\* P3.0 \*/

static const uint8\_t MISO = 14; /\* P3.1 \*/

Can someone help me troubleshoot where i am going wrong.

Thanks in advance.

```auto
// SPI Stuff here
#include "SPI.h"
const uint8_t MCP3911_CS = SS; // Teensy SPI CS1 = MCP3911

void setup() {

  //SPI Bus setup
  digitalWrite(MCP3911_CS,HIGH); //
  pinMode (MCP3911_CS, OUTPUT); // MCP3911

  
  SPI.setBitOrder(MSBFIRST);
  SPI.setDataMode(SPI_MODE0);
  SPI.setClockDivider(SPI_CLOCK_DIV8); //i.e. 6MHz on a Teensy running at 48MHz. 
  SPI.begin();

  //Setup Serial Comms
  Serial.begin(115200);
  Write_MCP3911_Register (0x0D, B11000010); 
}

int32_t adc;
void loop()
{
  //adc = Read_MCP3911_24bit(0x00);
  Read_MCP3911_Register(0x0D);
// Serial.print("Ch0 : ");
// Serial.println(adc);
  delay(200); 
}

uint8_t Write_MCP3911_Register (uint8_t MCP3911_Register_Address, uint8_t Command) {
  Serial.print("Command Register Received: ");
  Serial.print(MCP3911_Register_Address,HEX);
  Serial.print(" - Command Received: ");
  Serial.println(Command,BIN);

  MCP3911_Register_Address <<= 1; //left shift address one digit
  MCP3911_Register_Address &= B00111110; // and ensure last digit is a zero for write command
  digitalWrite(MCP3911_CS, LOW); // now take CS low to enable SPI device
  SPI.transfer(MCP3911_Register_Address); // send address with write command to MCP3911
  SPI.transfer(Command); //now send payload
  digitalWrite(MCP3911_CS, HIGH); // deselect the CS pin. 

  Serial.print(" Write Command Byte Sent: ");
  Serial.println(MCP3911_Register_Address,BIN); // verify what command was sent (i.e. address and write bit = 0)

  //Now Verify all went well. If so, have the function return value of one,
  //otherwise, alert the user that something is amiss. 
  uint8_t Response = Read_MCP3911_Register (MCP3911_Register_Address>>1);
  if (Response == Command) return 1;
  else 
  {
    Serial.println("");
    Serial.print("Error for register: ");
    Serial.print(MCP3911_Register_Address>>1,BIN);
    Serial.print(" - Command Sent: ");
    Serial.print(Command,BIN);
    Serial.print(" - Response Received: ");
    Serial.println(Response,BIN);
    Serial.println("");
    return 0;
  }
}

uint8_t Read_MCP3911_Register (uint8_t MCP3911_Register_Address) {
  
  MCP3911_Register_Address <<=1; //left shift address one bit for command byte 
  MCP3911_Register_Address |=1; // Ensure read bit is set
  
  Serial.print(" Read Byte Command Sent: ");
  Serial.print(MCP3911_Register_Address,BIN);
  
  digitalWrite(MCP3911_CS, LOW); 
  SPI.transfer(MCP3911_Register_Address); // send address with read command to MCP3911
  uint8_t Response = SPI.transfer(0x00); 
  digitalWrite(MCP3911_CS, HIGH);
 
  Serial.print(" - Response Received: ");
  Serial.println(Response,BIN);
  return Response;
}

void Reset_ADC()
{
 // Puts ADC into Reset Mode, i.e. stops ADC conversions until setup is complete.
  Write_MCP3911_Register (0x0D, B11000010); 
}

int32_t Read_MCP3911_24bit( uint8_t MCP3911_Register_Address)
  {
    uint8_t HB,MB,LB=0, MCP3911_CTRL=0;;
    int32_t adc0code=0;
    MCP3911_CTRL = 0;
    MCP3911_CTRL =(MCP3911_Register_Address<<1); //left shift address one digit for write command
    MCP3911_CTRL |= 1; //Turn on Read Operation by toggling last bit on
    
    digitalWrite(MCP3911_CS, LOW);
    SPI.transfer(MCP3911_CTRL); // send command byte to MCP3911
    HB = SPI.transfer(0x0);//receive High Byte
    MB = SPI.transfer(0x0);//receive Middle Byte
    LB = SPI.transfer(0x0);//receive Low Byte
    digitalWrite(MCP3911_CS, HIGH);
    
    adc0code = HB;
    adc0code = adc0code<<8;
    adc0code |= MB;
    adc0code = adc0code<<8;
    adc0code |= LB; //connecting the 3 bytes to one number
    
    
    return adc0code;// returning result
  }

```