# STM32: Can't get I2C to work

**URL:** <https://community.sparkfun.com/t/stm32-cant-get-i2c-to-work/13607>\
**Category:** MicroMod\
**Tags:** arm-lpc\
**Created:** [December 12, 2009, 12:26am UTC](https://community.sparkfun.com/t/stm32-cant-get-i2c-to-work/13607 "2009-12-12T00:26:43Z")\
**Posts on this page:** 7\
**Page:** 1

<div class="post-metadata">

**Author:** ![planius](https://avatars.discourse-cdn.com/v4/letter/p/94ad74/32.png) [@planius](https://community.sparkfun.com/u/planius)\
**Post date:** [December 12, 2009, 12:26am UTC](https://community.sparkfun.com/t/stm32-cant-get-i2c-to-work/13607/1 "2009-12-12T00:26:43Z")

</div>

Hi,

I am new to the STM32 and the Standard Peripheral library, so it’s quite likely the mistake I am making in getting I2C to work is simple, but I can’t see it.

I am using a ET-STM32 Stamp (bare metal) board with STM32F103RE6 CPU. I have connected PB6,7 (I2C1) to a LIS3LV02DQ 3-axis accelerometer, which has an I2C interface. I am using CrossWorks 2.0 and the STM32 Standard Peripheral Library V3.1.2.

The code below runs to the point in the first call to I2C\_LIS3L\_Write (from I2C\_LIS3L\_Init) where it checks for the EV5 event after I2C\_GenerateSTART. This test always fails, the only flag set in the I2C\_SR1/2 registers is BUSY. At that same point both the SDA line is low and SCL is high, I don’t see a clock signal on the DSO at all.

The datasheet for the LIS3LV02DQ says it incorporates pull-up resistors for SDA/SCL, which makes it seem odd that SDA is low?

I would welcome any hints on what I am doing wrong.

Thanks

Peter

```auto
/* Includes ------------ --------- --------- --------- --------- --------- -*/
#include "stm32f10x.h"

/* Defines for the GPIO pins used for the I2C communication */
#define I2C_LIS3L I2C1
#define I2C_LIS3L_CLK RCC_APB1Periph_ I2C1
#define I2C_LIS3L_GPIO GPIOB
#define I2C_LIS3L_GPIO_ CLK RCC_APB2Periph_ GPIOB
#define I2C_LIS3L_SCL GPIO_Pin_6
#define I2C_LIS3L_SDA GPIO_Pin_7

/* Define a structure for the 16bit Acceleration data */
typedef struct {
uint16_t X_Accel;
uint16_t Y_Accel;
uint16_t Z_Accel;
} LIS3L_AccelTypeDef;

// Physical Device Address - Factory Assigned to 0x3A for LIS3LV02DQ
#define LIS3L_SLAVE_ ADDR 0x3A
// The Who Am I register contains the physical device address
#define LIS3L_WHO_AM_ I 0x0F
// Define the Initialisation code as per the data sheet
#define LIS3L_INIT_CODE 0xC7
// Set CTRL_REG1 to Run Mode, 640Hz data rate and X,Y,Z enabled
#define LIS3L_RUN_CODE 0xE7

// Control registers
#define LIS3L_CTRL_REG1 0x20
#define LIS3L_CTRL_REG2 0x21

// Output data
// X axis acceleration data LSB
#define LIS3L_OUTX_L 0x28
// X axis acceleration data MSB
#define LIS3L_OUTX_H 0x29
// Y axis acceleration data LSB
#define LIS3L_OUTY_L 0x2A
// Y axis acceleration data MSB
#define LIS3L_OUTY_H 0x2B
// Z axis acceleration data LSB
#define LIS3L_OUTZ_L 0x2C
// Z axis acceleration data MSB
#define LIS3L_OUTZ_H 0x2D

/* Function Definitions ------------ --------- --------- --------- --------- ------- */
void I2C_LIS3L_Init( void);
uint8_t I2C_LIS3L_ReadByte( uint8_t ReadAddr);
void I2C_LIS3L_ReadAccel (uint8_t ReadAddr, LIS3L_AccelTypeDef* LIS3L_AccelStruct) ;
void I2C_LIS3L_Write( uint8_t WriteAddr, uint8_t DataByte);

/**
*********************  ******************  ******************  ****************** ***
* @file lis3l_i2c.c
* @author Peter Lanius
* @version V0.10
* @date 09/12/2009
* @brief This file provides functions to operate the LIS3LV02DQ 3-axis
accelerometer in I2C bus mode.
*********************  ******************  ******************  ****************** ***
* @copy
*/

/* Includes ------------ --------- --------- --------- --------- --------- -*/
#include "lis3l_i2c.h"
#include "stm32f10x_i2c. h"

/* Private typedef ------------ --------- --------- --------- --------- --------- -*/
/* Private define ------------ --------- --------- --------- --------- --------- -*/
#define I2C_Speed 100000 // 100kHz bus speed (up to 400kHz is ok)
#define I2C_SLAVE_ADDRESS7 0xA0 // I2C own address if in slave mode

/* Private macro ------------ --------- --------- --------- --------- --------- -*/
/* Private variables ------------ --------- --------- --------- --------- --------- */
/* Private function prototypes ------------ --------- --------- --------- --------* /
void GPIO_Configuration( void);
void I2C_Configuration( void);

/* Private functions ------------ --------- --------- --------- --------- --------- */

/**
* @brief Configure the used I/O ports pin
* @param None
* @retval None
*/
void GPIO_Configuration( void)
{
GPIO_InitTypeDef GPIO_InitStructure;

/* Configure I2C_LIS3L pins: SCL and SDA */
GPIO_InitStructure. GPIO_Pin = I2C_LIS3L_SCL | I2C_LIS3L_SDA;
GPIO_InitStructure. GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure. GPIO_Mode = GPIO_Mode_AF_ OD;
GPIO_Init(I2C_ LIS3L_GPIO, &GPIO_InitStructure );
}

/**
* @brief I2C Configuration
* @param None
* @retval None
*/
void I2C_Configuration( void)
{
I2C_InitTypeDef I2C_InitStructure;

/* I2C configuration */
I2C_InitStructure. I2C_Mode = I2C_Mode_I2C;
I2C_InitStructure. I2C_DutyCycle = I2C_DutyCycle_ 2;
I2C_InitStructure. I2C_OwnAddress1 = I2C_SLAVE_ADDRESS7;
I2C_InitStructure. I2C_Ack = I2C_Ack_Enable;
I2C_InitStructure. I2C_Acknowledged Address = I2C_AcknowledgedAdd ress_7bit;
I2C_InitStructure. I2C_ClockSpeed = I2C_Speed;

/* I2C Peripheral Enable */
I2C_Cmd(I2C_ LIS3L, ENABLE);

/* Apply I2C configuration after enabling it */
I2C_Init(I2C_ LIS3L, &I2C_InitStructure) ;
}

/**
* @brief Initializes peripherals used by the I2C LIS3L driver.
* @param None
* @retval None
*/
#define TxBuffer1Size (countof(TxBuffer1) - 1)
#define TxBuffer2Size (countof(TxBuffer2) - 1)

/* Private macro ------------ --------- --------- --------- --------- --------- -*/
#define countof(a) (sizeof(a) / sizeof(*(a)) )

void I2C_LIS3L_Init( )
{
uint8_t TxBuffer1[] = "\n\rLIS3LV02DQ Initialisation OK.\n\r";
uint8_t TxBuffer2[] = "\n\rLIS3LV02DQ Initialisation FAILED.\n\r" ;
uint8_t TxCounter = 0;
uint8_t lis3l_addr = 0;

/* I2C Periph clock enable */
RCC_APB1PeriphClock Cmd(I2C_LIS3L_ CLK, ENABLE);

/* GPIO Periph clock enable */
RCC_APB2PeriphClock Cmd(I2C_LIS3L_ GPIO_CLK, ENABLE);

/* GPIO configuration */
GPIO_Configuration( );

/* I2C configuration */
I2C_Configuration( );

/* Initialise the device as per data sheet */
I2C_LIS3L_Write( LIS3L_CTRL_ REG1, LIS3L_INIT_CODE) ;
I2C_LIS3L_Write( LIS3L_CTRL_ REG2, 0x00);

/* check everything is ok by reading whoami register */
lis3l_addr = I2C_LIS3L_ReadByte( LIS3L_WHO_ AM_I);
if(lis3l_addr == LIS3L_SLAVE_ ADDR) {
/* Match - Send the relevant message */
while(TxCounter+ + < TxBuffer1Size)
{
USART_SendData( USART1, TxBuffer1[TxCounter -1]);
while(USART_ GetFlagStatus( USART1, USART_FLAG_TXE) == RESET);
}
}
else {
/* Mismatch - Send the relevant message */
while(TxCounter+ + < TxBuffer2Size)
{
USART_SendData( USART1, TxBuffer2[TxCounter -1]);
while(USART_ GetFlagStatus( USART1, USART_FLAG_TXE) == RESET);
}
}

/* Set the data rate to the desired rate */
I2C_LIS3L_Write( LIS3L_CTRL_ REG1, LIS3L_RUN_CODE) ;
}

/**
* @brief Write a byte to the specified register of the LIS3L sensor
* @param WriteAddr : 8bit write address of the LIS3L register
* @param DataByte : byte to write to the specified register
* @retval none
*/
void I2C_LIS3L_Write( uint8_t WriteAddr, uint8_t DataByte)
{
/* Send STRAT condition */
I2C_GenerateSTART( I2C_LIS3L, ENABLE);

/* Test on EV5 and clear it */
while(!I2C_CheckEve nt(I2C_LIS3L, I2C_EVENT_MASTER_ MODE_SELECT) );

/* Send LIS3L address for write */
I2C_Send7bitAddress (I2C_LIS3L, LIS3L_SLAVE_ ADDR, I2C_Direction_ Transmitter) ;

/* Test on EV6 and clear it */
while(!I2C_CheckEve nt(I2C_LIS3L, I2C_EVENT_MASTER_ TRANSMITTER_ MODE_SELECTED) );

/* Send the LIS3L's internal register address to write to */
I2C_SendData( I2C_LIS3L, WriteAddr);

/* Test on EV8 and clear it */
while(!I2C_CheckEve nt(I2C_LIS3L, I2C_EVENT_MASTER_ BYTE_TRANSMITTED ));

/* Send the byte to be written */
I2C_SendData( I2C_LIS3L, DataByte);

/* Test on EV8 and clear it */
while(!I2C_CheckEve nt(I2C_LIS3L, I2C_EVENT_MASTER_ BYTE_TRANSMITTED ));

/* Send STOP condition */
I2C_GenerateSTOP( I2C_LIS3L, ENABLE);
}

```

---

<div class="post-metadata">

**Author:** ![MichaelN](https://avatars.discourse-cdn.com/v4/letter/m/b19c9b/32.png) [@MichaelN](https://community.sparkfun.com/u/MichaelN)\
**Post date:** [December 12, 2009, 6:56am UTC](https://community.sparkfun.com/t/stm32-cant-get-i2c-to-work/13607/2 "2009-12-12T06:56:54Z")

</div>

Sorry, I don’t have time to go through your code, but I assume you are holding pin 19 (CS) on the accelerometer HIGH (ie, to select I2C mode)?

It wouldn’t hurt to put pullup resistors (say 10K) on the SDA and SCL if you’re measuring a low voltage - it is possible that the datasheet was wrong about the pullup resistors. It’s much more likely that something in your code is holding the lines low though.

---

<div class="post-metadata">

**Author:** ![planius](https://avatars.discourse-cdn.com/v4/letter/p/94ad74/32.png) [@planius](https://community.sparkfun.com/u/planius)\
**Post date:** [December 12, 2009, 7:58am UTC](https://community.sparkfun.com/t/stm32-cant-get-i2c-to-work/13607/3 "2009-12-12T07:58:08Z")

</div>

Yes, I am holding CS HIGH via a pull-up resistor.

I have also tried adding external pull-up resistors to SDA and SCL. The result is the same (it stops at the same point), but now the following flags are set in I2C\_SR1/2: BUSY, BERR and STOPF. So the only effect is to add a bus error and stop flag to something that wasn’t working in the first place…

---

<div class="post-metadata">

**Author:** ![planius](https://avatars.discourse-cdn.com/v4/letter/p/94ad74/32.png) [@planius](https://community.sparkfun.com/u/planius)\
**Post date:** [December 13, 2009, 9:41am UTC](https://community.sparkfun.com/t/stm32-cant-get-i2c-to-work/13607/4 "2009-12-13T09:41:39Z")

</div>

OK, I have done some more tests:

- I can run the I2C sample code that comes with the Standard Peripheral Library where I2C1 talks to I2C2

- I can’t talk to the LIS3LV02DQ using my Bus Pirate. Admittedly, I haven’t used the Bus Pirate before, but it seemed easy enough to set up and talk to via Terminal. It can’t see the accelerometer in I2C mode when performing a bus scan or when talking directly to the correct address.

Makes me wonder if the accelerometer works, but it’s new and I bought it from Sparkfun 😉

---

<div class="post-metadata">

**Author:** ![kk6gm](https://avatars.discourse-cdn.com/v4/letter/k/cc9497/32.png) [@kk6gm](https://community.sparkfun.com/u/kk6gm)\
**Post date:** [December 13, 2009, 4:53pm UTC](https://community.sparkfun.com/t/stm32-cant-get-i2c-to-work/13607/5 "2009-12-13T16:53:55Z")

</div>

Just checking the obvious, are your supply and ground connections correct? Do you have the I2C mode selected (pin 13 high)?

---

<div class="post-metadata">

**Author:** ![planius](https://avatars.discourse-cdn.com/v4/letter/p/94ad74/32.png) [@planius](https://community.sparkfun.com/u/planius)\
**Post date:** [December 14, 2009, 7:08am UTC](https://community.sparkfun.com/t/stm32-cant-get-i2c-to-work/13607/6 "2009-12-14T07:08:37Z")

</div>

Yes, the whole thing lives as a prototype on a bread board right now and I have checked all the pins with the DSO and the logic probe…

I also have a HMC5843 magnetic sensor, which also uses an I2C interface, so I am going to try that one over the next few days. This should settle if it’s an issue with the initialisation code or hardware.

---

<div class="post-metadata">

**Author:** ![jramirez](https://avatars.discourse-cdn.com/v4/letter/j/e95f7d/32.png) [@jramirez](https://community.sparkfun.com/u/jramirez)\
**Post date:** [June 8, 2010, 6:09pm UTC](https://community.sparkfun.com/t/stm32-cant-get-i2c-to-work/13607/7 "2010-06-08T18:09:24Z")

</div>

I am having the same issue when talking to the 24lc1025 i2c eeprom. After I send the Generate start I see that the status registers come back with this code 0x00020000 ( this is ( (SR2\<\<16) & SR1 ) ) I have exactly the same set up as posted above any ideas.