# STM32F103RE + Stlink v2 + offseting past a bootloader

**URL:** <https://community.sparkfun.com/t/stm32f103re-stlink-v2-offseting-past-a-bootloader/30954>\
**Category:** MicroMod\
**Tags:** arm-lpc\
**Created:** [May 24, 2015, 3:41pm UTC](https://community.sparkfun.com/t/stm32f103re-stlink-v2-offseting-past-a-bootloader/30954 "2015-05-24T15:41:07Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![sd\_tom](https://avatars.discourse-cdn.com/v4/letter/s/a9adbd/32.png) [@sd\_tom](https://community.sparkfun.com/u/sd_tom)\
**Post date:** [May 24, 2015, 3:41pm UTC](https://community.sparkfun.com/t/stm32f103re-stlink-v2-offseting-past-a-bootloader/30954/1 "2015-05-24T15:41:07Z")

</div>

Ok i’m trying to use OpenOCD within VisualGDB (I don’t think this is a visualGDB thing just yet, short of not being able to upgrade to 0.9.0 just yet). This is with a STM32F103RE (64k RAM, 512KB ROM) I have an image i’m trying to debug. It is offset 0x3000; bringing that up just in case… openocd logs seem to recognize it though, just not working. I can flash the image via the stlink utility, works fine. Any thoughts? Is this something that would improve with 0.9.0?

**Command Line:**

openocd.exe -f interface/stlink-v2.cfg -f target/stm32f1x\_stlink.cfg -c init -c “reset init”

**Log:**

```auto
Open On-Chip Debugger 0.8.0 (2014-05-02-12:11)
Licensed under GNU GPL v2
For bug reports, read
        http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : This adapter doesn't support configurable speed
Info : STLINK v2 JTAG v23 API v2 SWIM v4 VID 0x0483 PID 0x3748
Info : using stlink api v2
Info : Target voltage: 3.205243
Info : stm32f1x.cpu: hardware has 6 breakpoints, 4 watchpoints
target state: halted
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x080028d0 msp: 0x20000a30
Info : accepting 'gdb' connection from 3333
Info : device id = 0x10036414
Info : flash size = 512kbytes
target state: halted
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x080028d0 msp: 0x20000a30
target state: halted
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x080028d0 msp: 0x20000a30
target state: halted
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x080028d0 msp: 0x20000a30
Info : Padding image section 0 with 4 bytes
Info : Padding image section 1 with 412852 bytes
Error: flash write algorithm aborted by target
Error: flash write failed at address 0x801b002
Error: flash memory not erased before writing
Error: error writing to flash at address 0x08000000 at offset 0x00003000
Warn : keep_alive() was not invoked in the 1000ms timelimit. GDB alive packet not sent! (2990). Wo
rkaround: increase "set remotetimeout" in GDB
target state: halted
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x080028d0 msp: 0x20000a30

```

**\*\*Scripts (standard i think / unless visualgdb guys changed):\*\***

_stlink-v2.cfg_

```auto
#
# STMicroelectronics ST-LINK/V2 in-circuit debugger/programmer
#

interface hla
hla_layout stlink
hla_device_desc "ST-LINK/V2"
hla_vid_pid 0x0483 0x3748

```

_stm32f1x\_stlink.cfg_

```auto
#
# STM32f1x stlink pseudo target
#

if { [info exists CHIPNAME] == 0 } {
   set CHIPNAME stm32f1x
}

if { [info exists CPUTAPID] == 0 } {
   set CPUTAPID 0x1ba01477
}

if { [info exists WORKAREASIZE] == 0 } {
   set WORKAREASIZE 0x1000
}

source [find target/stm32_stlink.cfg]

set _FLASHNAME $_CHIPNAME.flash
flash bank $_FLASHNAME stm32f1x 0 0 0 0 $_TARGETNAME

```

_stm32\_stlink.cfg_

```auto
#
# stm32 stlink pseudo target
#

if { [info exists CHIPNAME] } {
   set _CHIPNAME $CHIPNAME
} else {
   set _CHIPNAME stm32f1x
}

# Work-area is a space in RAM used for flash programming
# By default use 4kB (as found on some STM32F100s)
if { [info exists WORKAREASIZE] } {
   set _WORKAREASIZE $WORKAREASIZE
} else {
   set _WORKAREASIZE 0x1000
}

if { [info exists CPUTAPID] } {
   set _CPUTAPID $CPUTAPID
} else {
   # this is the SW-DP tap id not the jtag tap id
   set _CPUTAPID 0x1ba01477
}

if { [info exists TRANSPORT] } {
   set _TRANSPORT $TRANSPORT
   if { $TRANSPORT == "hla_jtag" } {
      if { [info exists CPUTAPID] == 0 } {
         # jtag requires us to use the jtag tap id
         set _CPUTAPID 0x3ba00477
      }
   }
} else {
   set _TRANSPORT hla_swd
}

# add deprecated transport name check
if { $_TRANSPORT == "stlink_swd" } {
	set _TRANSPORT "hla_swd"
	echo "DEPRECATED! use 'hla_swd' transport not 'stlink_swd'"
}

if { $_TRANSPORT == "stlink_jtag" } {
	set _TRANSPORT "hla_jtag"
	echo "DEPRECATED! use 'hla_jtag' transport not 'stlink_jtag'"
}
# end deprecated checks

#
# possibles value are hla_swd or hla_jtag
#
transport select $_TRANSPORT

hla newtap $_CHIPNAME cpu -expected-id $_CPUTAPID

set _TARGETNAME $_CHIPNAME.cpu
target create $_TARGETNAME hla_target -chain-position $_TARGETNAME

$_TARGETNAME configure -work-area-phys 0x20000000 -work-area-size $_WORKAREASIZE -work-area-backup 0

```

---

<div class="post-metadata">

**Author:** ![sd\_tom](https://avatars.discourse-cdn.com/v4/letter/s/a9adbd/32.png) [@sd\_tom](https://community.sparkfun.com/u/sd_tom)\
**Post date:** [May 26, 2015, 3:23am UTC](https://community.sparkfun.com/t/stm32f103re-stlink-v2-offseting-past-a-bootloader/30954/2 "2015-05-26T03:23:54Z")

</div>

Ok somehow it went away. Changing too many variables to know for sure:

- upgraded to 0.9.0

- borrowed 0.9.0 nucleo-f103 scripts

- increased working space

- went to true stlink driver (got rid of winusb)

- erased the chip and replaced boot loader with st link utility (st link wasn’t recognized by utility with other driver)