# STR-E912 Development-Board and CAN (Controller Area Network)

**URL:** <https://community.sparkfun.com/t/str-e912-development-board-and-can-controller-area-network/16661>\
**Category:** MicroMod\
**Tags:** arm-lpc\
**Created:** [July 20, 2010, 5:37pm UTC](https://community.sparkfun.com/t/str-e912-development-board-and-can-controller-area-network/16661 "2010-07-20T17:37:03Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![ChristophNiemann](https://avatars.discourse-cdn.com/v4/letter/c/aca169/32.png) [@ChristophNiemann](https://community.sparkfun.com/u/ChristophNiemann)\
**Post date:** [July 20, 2010, 5:37pm UTC](https://community.sparkfun.com/t/str-e912-development-board-and-can-controller-area-network/16661/1 "2010-07-20T17:37:03Z")

</div>

Hi everybody,

I’m quite new in developing Software for Software for the STR912FW44 from ST.

I’m using an Olimex Development Board (STR-E912) wich also contains a CAN Controller.

I was able to find an example from Hitex [[here](http://www.hitex-download.de/examples/st/str9/str9-comstick/AP-ARM-0112.zip) wich implements sending

a CAN Message, but was for the STR9-comstick. However, I managed to compile the Software (later with a blinking LED to confirm the Software is working) an

flash it to the STR9. The Problem is: There is nothing on the CAN. On Problem should be, that the CAN-TX is on a GPIO-Pin, wich is not connected to the phyisical

CAN-Interface of the Board. But I was not able to Measure any change (using an oscilloscpe) anywhere on the Board. In the end i was switching on the LED, when

starting to send something and switch it of, when finished. I noticed, that it was taking longer, when i uncommented the sending off a CAN Message.

Now i have no clue where to search next, since i can measure nothing. I would be really happy, if someone could help me out.

I used arm-elf-gcc 3.4.4 under Debian Testing for compiling.

Cheers

Christoph

```auto
/* Main Program */
int main(void)
{

// stuff for blinking
// turn on clock for GPIO port 9
SCU_PCGR1 = BIT23;
// take port out of reset
SCU_PRR1 = BIT23;
P9DIR = 1; // make LSB an output

//config für CAN
SCU_Configuration();
CAN_Configuration();

while (1)
   {     
      P9LSB = 1; // on
      //for (inner=0;inner < 5;inner++);
      //ReallyLongDelay();
      CAN->sMsgObj[0].DA1R = 0x22 ;
      /* Set the message valid bit */
      /* Update informations from interface registers */
      CAN->sMsgObj[0].CRR = 2;
      P9LSB = 0; // off
      ReallyLongDelay();
   }

}

void ReallyLongDelay() {
	long inner;
		for (inner=0;inner < 1000;inner++);
}

void SCU_Configuration (void)
{
   // Initialise STR912 CPU
   // All SCU-PCGR1 peripherals clocks are disabled by default in START912.S
   // Do not clear any bits in SCU_PCGR0 as this is the SRAM, VIC etc!
   SCU->PCGR1 |= (SCU->PCGR1 & ~0x00080000) | 0x00080000 ; /* Clock for GPIO5 is b19 */
   SCU->PRR1 &= ~0x00080000 ; /* Force reset */
   SCU->PRR1 |= 0x00080000 ; /* Release reset */

   SCU->GPIOOUT[5] = 0x0008 ; /* P5.0 = alt input 1, P5.1 = alt output 2 */
   SCU->GPIOIN[5] = 0x03 ; /* P5.0 = alt input 1 */
   SCU->GPIOTYPE[5] = 0x0000 ; /* All output pins are push-pull */
   GPIO5->DDR = 0x02 ; /* No simple IO used */

   /* Initialise CAN Module */
   /* Enable CAN peripheral clocks */
   SCU->PCGR1 |= (SCU->PCGR1 & ~0x00000400) | 0x00000400 ; /* Clock for CAN is b10 */
   SCU->PRR1 &= ~0x00000400 ; /* Force reset */
   SCU->PRR1 |= 0x00000400 ; /* Release reset */
   /* Set APBDIV to get 48MHz PCLK */
   SCU->CLKCNTR = (SCU->CLKCNTR & ~0x00000180) | 0x00000080 ; /* PCLK = Fmstr/2 = 48MHz */
}
void CAN_Configuration (void)
{
   /* Initialise CAN0 for full (part2.0B) CAN operation */
   CAN->CR = 0x00000001; /* init and config change enable */
   CAN->CR = 0x000000C1;
   CAN->BRPR = 0x00000000; /* Clear the extended BRP */

// CAN->BTR = 0x00003AC5; /* Set bit rate to 500K: Tq = PCLK/24 = 0.5us, TSEG1 = 9, TSEG2 = 4, SJW = 4 */
   CAN->BTR = 0x0000755F; /* Set bit rate to 100K */
   CAN->CR = 0x00; /* End CAN initialisation mode */

   CAN->sMsgObj[0].CMR = 0x00B3;
   /* Reset the MSGVAL bit to enable ID, DIR and DLC change */
   CAN->sMsgObj[0].A2R = 0;
   /* Setup the identifier information */
   CAN->sMsgObj[0].A1R = 0x00;
   CAN->sMsgObj[0].A2R = 0x04;
   /* Setup type information */
   CAN->sMsgObj[0].A2R |= CAN_A2R_DIR|CAN_A2R_XTD;

   /* Setup data bytes */
   CAN->sMsgObj[0].MCR = 0x8980 | 1;

   CAN->sMsgObj[0].A2R |= CAN_A2R_MSGVAL;
}

```

]([Der Domainname hitex-download.de steht zum Verkauf.](http://www.hitex-download.de/examples/st/str9/str9-comstick/AP-ARM-0112.zip))