Hi all,
The situation has changed a bit since a last meeting.
Given that we need to also stream the data from the car back to the person with the VR-set, we plan on installing a 4G/5G router on the car. This enables the use of NTRIP. Reading through the forum, this is a more ‘easy’ setup than always configuring your own base.
That still leaves the choice of rover open. The update rate has become more important than initially thought, which is why we are leaning to the mosaic-X5 (100Hz). All the facet-FP’s only reach 20Hz (even with mosaic-X5 core).
My question is whether the following setup will work, or if I’m overlooking problems. Also, what would be the main reasons to switch to the facet FP instead of the mosaic-X5?
RTK/GNSS sensor on car, receiving RTK corrections over NTRIP from a 4G/5G router.
The sensor sends its position over wifi to a stationary laptop, which processes the data and is connected to the VR-set.
Thank you for the help!