"MJPEG in AVIs having the MJPG fourcc, is restricted JPEG with a fixed – and omitted – Huffman table. The JPEG must be YCbCr colorspace, it must be 4:2:2, and it must use basic Huffman encoding, not arithmetic or progressive. "
This means it should be quite easy to get the cam to output right format as long as you can force the huffman table to standard and then omit it in the stream.
I edited my previous message about HCOUNT and VCOUNT calculations.
Here is what I added (although it still may not be correct):
buffercam:
It seems that the HCOUNT calculation is based on counting the clocks in a single row of image data at 1/2 the DSP clock frequency.
So for the Full Mega size, note that the data output is output at 1 x DSP frequency. This means you divide the number of clocks by two when calculating HCOUNT.
Smaller images are output at 1/4 the DSP clock rate, so you need to multiply the number of clocks by 2.
The result is that for every picture size, HCOUNT comes out to be approximately the default value of 713 (after you subtract the offset of 677). (I actually calculate 715.)
I also wish there were better docs. All we know are whats in the appnote together with the list of names and addresses in the datasheet.
what HCOUNT actually does appears to be a bit vague.
I have issues with my cams not delivering the entire frame and suspect this to be a small setting-error simply due to poor docs.
Best I can do is adjust so I get about half a image. Still, the image is then completely wrong colorwise. It’s like it’s YUV or something even though RGB is active.
Are you sure your camera is outputting at 15 fps (the maximum output rate specified in the datasheet)?
My camera tries to output at 30 fps when the frame rate is set to the max.
We have three settings for FRMSPD (specified in the Application Note):
Max frame rate
Half frame rate
Quarter frame rate
The datasheet only specified two frame rates: 15fps and 7.5fps.
Based on what I’ve measured, I think this is the relationship between the two:
Max frame rate = 30 fps, doesn’t work properly?
Half frame rate = 15 fps
Quarter frame rate = 7.5 fps
Perhaps they initially designed the camera to do 30 fps, but couldn’t get it to work in hardware, so they changed the datasheet to say 15 fps (instead of 30 fps)?
At any rate, try setting frame speed to “Half frame rate.”
I have been using lowest framerate as I am focusing on still capture to start with. What settings are you guys using for the rest of the parameters? Like RGB/YUV and audo-contrast/exposure…
Basically, the pink stuff on the left side is over-exposed and with wrong colors. If you take into account me not setting the exposure that leaves the right side black on my shot and the left hidiously pink!
I think I’ll have to play around a bit to get this right but wohooo!
The AppNote says SPCOUNT = 2 x (H_COUNT + 191) for that PICSIZ. That’s different than what you used.
Also, what is Register 0x0E?
0x02 0x00 //Set Camera Active (I assume you did this?)
0x0B 0x00 // White Line OFF
0x58 0x20 // Exposure Time
0x05 0x00 // Frame Rate Quarter
0x1A 0xFF // HCOUNT = 0x3FF = 1023
0x1B 0xB3 // VCOUNT = 0x21B = 539 // Assuming Register 0x1C is left at the default (0xA1)
0x11 0x4A // Changed b/c of PICSIZE
0x14 0x33 // Changed b/c of PICSIZE
0x04 0x0D // RGB 352x288 OUT ON
0x1F 0x0B // SPCOUNT = 0xBC3 = 3011 // Doesn't match formula?
0x1E 0xC3 // SPCOUNT[7:0]
0x0E 0x1E // According to the AppNote it should be 0xAC for this PICSIZ?
I’ve been following this thread… although I haven’t been able to get to play with my camera yet… I’m (relatively) new to electronics and think given all the experimentation and hard work I’ve seen you guys doing that I may have bitten off a bit more than I can chew with this project that I’d like to do. I’m an artist in grad school and have been working on a project I call ‘Stop Motion Day’ with a super 8 camera for the last several months. For the project I made a harness to strap the super 8 to my body and set up the camera so that it records one frame every 16 seconds (the time lapse required to exactly record a waking day of 16 hours on a single roll of film). I’ve been struggling with trying to create a wearable digital version of this… ideally small enough to wear almost every day (where the super 8 is quite cumbersome and really a performance). I have the camera, a miniSD card and a lilypad… and would love to connect them and set them up to do a similar thing digitally. I’m appealing to this forum to see if anyone would be interested in helping me build this apparatus much more quickly than I can hope to do it alone. I’d be open to collaboration on the art piece or I can pay for a finished product. Any takers? Any suggestions?
A lillypad really isn’t appropriate for this camera, you’d need both something considerably more powerful and a fair bit of programming know-how. I’d advise getting a normal small and cheap digital camera and connecting the lillypad to its remote shutter so the lillypad tells it to take a photo every 16 seconds and it does all the photographing and storing for you - much much easier with much better results.
Thank you for the advice Random. I’ve considered this and run into two problems… one, many of the smallest cameras do not have expandable memory, so I wouldn’t know how to store all the images (roughly 3600 @ 16 seconds). I was looking at this one- http://www.target.com/Aiptek-Mini-PenCa … era&page=1.
And, then there’s the battery life, many of the cameras I looked at, since they wouldn’t effectively ‘sleep’ between shots, would go through their batteries in much less than 16 hours.
Any suggestions for how to get around these problems?