Codlinks & Mee_n_Mac
I,m back again. I’ve been going round and round trying to create a sketch using MultiWii V2.3 and Arduino 1.0.5-r2. I was trying to compile a sketch for sections 1 thru 8 of config_h_ of MW V2.3 by defining the setup and loop in the main.cpp tag of Arduino 1.0.5-r2 and I keep getting the error from the “;” after the “setup” in the main.cpp tag. What am I doing wrong?
Here is the main tag as I have changed it, and also the error that I get trying to compile the tag.
#include <Arduino.h>
int main(void)
{
init();
#if defined(USBCON)
USBDevice.attach();
#endif;
setup();
1 for (config_h_ ) {
8 loop();
if (serialEventRun) serialEventRun(); }
return 0;
}
C:\Documents and Settings\HP_Administrator\Desktop\arduino-1.0.5-r2\hardware\arduino\cores\arduino\main.cpp: In function 'int main()':
C:\Documents and Settings\HP_Administrator\Desktop\arduino-1.0.5-r2\hardware\arduino\cores\arduino\main.cpp:13: error: expected `;' before 'for'
[code]