Is there a possibility that, for Wav Trigger / Tsunami, have loop start and end points ? I am building a synth project which really needs this future.
As I understand, now it only loops within the whole wav file no points are configurable.
On some projects there is no need to have a loooooooooong version of the file and just looping a wav file after the “attack” part of the sample. especially organ and pad style sounds.
anyway, is there a progress about it ? Thanks.
A post from a few years ago touches on this…Tsunami has seamless looping, but that isn’t the same as adding user-defined loop points :-/
It might be something that gets added in a future firmware release though
The Robertsonics polyphonic audio players differ from most other sample players in that they stream audio directly from microSD, using only the limited amount of RAM in the MCU. This keeps them simple and immune from RAMageddon, but it also imposes some access rules that make arbitrary loop point awkward at best. It was a challenge simply to provide seamless looping around an arbitrary file length with Tsunami. It’s unlikely that either the WAV Trigger or Tsunami will ever support user defined loop points. Just want to be up front about that.
The newer WAV Trigger Pro, however, was designed to be able to eventually support this. But I don’t have a timeframe, and sales of this product have been somewhat lackluster, so it’s not a priority.