Unable to Find BLE Shield

Hi everyone,

I’m currently trying to run the MyoWare BLE Central (Artemis Nano) – Robust Version code with my MyoWare BLE peripheral sensors. When running the envelope signal, I consistently encounter an issue where the sensors are not being detected by the microcontroller.

My sketches upload successfully without any errors; however, when I open the Serial Monitor, the sensors are not being discovered or connected.

System details:

Board: RedBoard Artemis Nano

OS: Windows 11 Pro

Port: COM4 (only port that successfully uploads code)

Troubleshooting steps I’ve tried:

Connected shields individually and together

Verified correct board selection

Ensured all components are fully charged and powered on

Assigned unique names to each sensor (“MyoWare Sensor 1” and “MyoWare Sensor 2”)

Updated the Central code to match these names

Despite this, the Central device is still unable to discover the sensors, and I continue to receive errors (listed below).

**!������% **


**MyoWare BLE Central (Robust) **


**---------------------------- **


**Scanning for service UUID: EC3AF789-2154-49F4-A9FC-BC6C88E9E930 **


**��~�� **


**MyoWare BLE Central (Robust) **



**---------------------------- **


**Scanning for service UUID: EC3AF789-2154-49F4-A9FC-BC6C88E9E930 **


**No MyoWare Wireless Shields found! **


**MyoWare BLE Central (Robust) **


**---------------------------- **


**Scanning for service UUID: EC3AF789-2154-49F4-A9FC-BC6C88E9E930 **


No MyoWare Wireless Shields found!

Has anyone run into this issue or have suggestions for additional troubleshooting steps?

Thanks in advance for any help.

Which myoware sensors do you have?

What is ‘Robust’ version?