# Uploading test file to SDcard

**URL:** <https://community.sparkfun.com/t/uploading-test-file-to-sdcard/23090>\
**Category:** Arduino\
**Created:** [January 19, 2012, 10:40pm UTC](https://community.sparkfun.com/t/uploading-test-file-to-sdcard/23090 "2012-01-19T22:40:00Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![UTwiald](https://avatars.discourse-cdn.com/v4/letter/u/f07891/32.png) [@UTwiald](https://community.sparkfun.com/u/UTwiald)\
**Post date:** [January 19, 2012, 10:40pm UTC](https://community.sparkfun.com/t/uploading-test-file-to-sdcard/23090/1 "2012-01-19T22:40:00Z")

</div>

Hello,

I am trying to upload the test file on Sparkfun’s website to a microSD card. I am using an ArduinoUNO and the Sparkfun SD shield. The code compiles fine on my computer but the test file will not show up on the microSD card when I try to access it. I saved the SDfat library in Documents\>Arduino\>libraries\>SdFat. I am not sure if there is an error in where the library is being saved or where my test code is being saved. Right now I have it saved in the libraries folder but have tried a few other places as well. Thanks for the help.

The code I am using from the Sparkfun website is below:

//Add the SdFat Libraries

#include \<SdFat.h\>

#include \<SdFatUtil.h\>

#include \<ctype.h\>

//Create the variables to be used by SdFat Library

Sd2Card card;

SdVolume volume;

SdFile root;

SdFile file;

char name = “Test.txt”; //Create an array that contains the name of our file.

char contents[256]; //This will be a data buffer for writing contents to the file.

char in\_char=0;

int index=0; //Index will keep track of our position within the contents buffer.

void setup(void)

{

Serial.begin(9600); //Start a serial connection.

pinMode(10, OUTPUT); //Pin 10 must be set as an output for the SD communication to work.

card.init(); //Initialize the SD card and configure the I/O pins.

volume.init(card); //Initialize a volume on the SD card.

root.openRoot(volume); //Open the root directory in the volume.

}

void loop(void){

file.open(root, name, O\_CREAT | O\_APPEND | O\_WRITE); //Open or create the file ‘name’ in ‘root’ for writing to the end of the file.

sprintf(contents, "Millis: %d ", millis()); //Copy the letters 'Millis: ’ followed by the integer value of the millis() function into the ‘contents’ array.

file.print(contents); //Write the ‘contents’ array to the end of the file.

file.close(); //Close the file.

file.open(root, name, O\_READ); //Open the file in read mode.

in\_char=file.read(); //Get the first byte in the file.

//Keep reading characters from the file until we get an error or reach the end of the file. (This will output the entire contents of the file).

while(in\_char \>=0){ //If the value of the character is less than 0 we’ve reached the end of the file.

Serial.print(in\_char); //Print the current character

in\_char=file.read(); //Get the next character

}

file.close(); //Close the file

delay(1000); //Wait 1 second before repeating the process.

}

---

<div class="post-metadata">

**Author:** ![rasmadrak](https://avatars.discourse-cdn.com/v4/letter/r/b5ac83/32.png) [@rasmadrak](https://community.sparkfun.com/u/rasmadrak)\
**Post date:** [January 20, 2012, 2:06pm UTC](https://community.sparkfun.com/t/uploading-test-file-to-sdcard/23090/2 "2012-01-20T14:06:27Z")

</div>

Usually the files are only written to “disc” when a SYNC is called. So you should probably do a file.flush() (If that’s the correct command) or maybe even file.sync().

Sort of like a SQL “commit”.