# will it work ?

**URL:** <https://community.sparkfun.com/t/will-it-work/12010>\
**Category:** SparkFun Site Questions/Comments\
**Created:** [July 26, 2009, 8:24am UTC](https://community.sparkfun.com/t/will-it-work/12010 "2009-07-26T08:24:32Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![jolie](https://avatars.discourse-cdn.com/v4/letter/j/e95f7d/32.png) [@jolie](https://community.sparkfun.com/u/jolie)\
**Post date:** [July 26, 2009, 8:24am UTC](https://community.sparkfun.com/t/will-it-work/12010/1 "2009-07-26T08:24:32Z")

</div>

Hi everyone

I’m building a robot , one of its main function is to do the following :

Go to a predefined destinations.I don’t want to Use path-follower because it clashes with another main function( avoiding obstacles ) . So i figured , one way to do this , is to get several (Transmitter\Receiver) pairs with different frequency for each pair.I’ll place Transmitter1 in destination1 , Tarnsmitter2 in destination2 etc. and place all the receivers in the robot.So when Receiver1 is activated the robot will go toward Transmitter1 (destination1) and so on .

My Questions are :

can i do that using :

RF Link 2400bps Receiver - 434MHz) & RF Link Transmitter - 434MHz

and

RF Link 2400bps Receiver - 315MHz & RF Link 2400bps Receiver - 315MHz

?

can i get a third pair with different frequency ?

Thanks in advanced 🙂

---

<div class="post-metadata">

**Author:** ![qema](https://avatars.discourse-cdn.com/v4/letter/q/a6a055/32.png) [@qema](https://community.sparkfun.com/u/qema)\
**Post date:** [July 26, 2009, 5:08pm UTC](https://community.sparkfun.com/t/will-it-work/12010/2 "2009-07-26T17:08:51Z")

</div>

Why don’t you try hooking up the transmitter to a micro controller, then you could have as many as you want (as long as they are flashign at different speeds).

You could also try to create a “lighthouse” like transmitter.

That way your robot would know what angle it is in reference to the transmitter.

[http://en.wikipedia.org/wiki/VHF\_omnidirectional\_range](http://en.wikipedia.org/wiki/VHF_omnidirectional_range)

This is one of they ways that aircraft find the airport.