WRL-18569 Datasheet

Hello,

I’m looking at using WRL-18569 (u.fl to RP-SMA cable).

I was wondering if there is an available datasheet for this product?

Or possibly the original manufacturer, so I can look for a datasheet with them.

Thank you,

I poked around a bit and couldn’t find one; we’ll email the manufacturer and see if they’ll send one over :slight_smile:

Thank you!

I look forward to their reply.

Hi Russell,

Just checking in. Any updates on this?

Not yet but hopefully shortly…usually takes a few days for them to respond

BCCA3315.pdf (82.5 KB)
Here goes :slight_smile:

Thank you Russell! This includes all the mechanical specs I was looking for.

Do they have any information on temperature rating and voltage rating? I’m discussing a product design with UL and those are the last two specifications they’re asking for.

BCCA3315 UL.pdf (287.6 KB)
It doesn’t have much on it but yes, they actually sent the UL too

This is very helpful thank you. I looked into UL758 and this product at UL Product iQ. It does give me the maximum voltage rating as 30VAC. The most recent document you shared also points to AWM styles 1354, 10871, and 11149; which gives me a general idea of the maximum temperature for the rating.

Style 1354: 60 or 80C, 30VAC

Style 10871: 80C, 30VAC

Style 11149: 200C, 30VAC

Looking at the specifications in the drawing you previously provided, I’m fairly certain that WRL-18569 is AWM style 1354. Which means this cable assembly should have either a max temperature rating of 60C or 80C. Could you confirm if the maximum temperature rating is 80C?

Thank you for all your help!

Wahoo!

I can ask but I wouldn’t hold my breath…if it is critical you might try 2 test spots on a unit and see if 60c causes damage :slight_smile:

Okay, while you’re waiting to hear back from the manufacturer I will see if there is any testing I can do on my end.