Trying to connect to XM125 pulsed radar breakout board. Using the Auctioneer Explorer tool. The CH340 driver is showing up in device manager. I plug the board in and see port 11 on serial. I set the baud to 115200, no flow control (doesnt work with flow either). but I get a recv timeout, failed to connect error, log is below. Tried flashing, same problem. What am I missing? A few things may have changed since the support section was published on this board. Also installed the CP210 driver but am not seeing the two virtual ports. Really out of options on why this won’t connect.
C
Checklist before reporting a bug
- I have read the ‘Common Issues’ without finding a solution
(See Common Issues — Acconeer docs ) - This issue occured in the latest release of Exploration Tool
(See acconeer-exptool · PyPI ) - I have double-checked that the section ‘Installed Packages’ contains
rows on the format ‘==’
Python version
3.12.16 (main, Oct 26 2026, 14:10:56) [MSC v.1944 64 bit (AMD64)]
Installed Packages
acconeer-exptool==7.18.2
attributes-doc==0.4.0
attrs==26.1.0
beautifulsoup4==4.15.0
bs4==0.0.2
cbor2==6.1.5
certifi==2026.10.23
charset-normalizer==3.5.2
colorama==0.4.6
commonmark==0.9.2
contourpy==1.4.0
cycler==0.12.1
darkdetect==0.7.1
docutils==0.23
exceptiongroup==1.1.1
fonttools==4.68.0
h5py==3.16.0
idna==3.20
importlib_resources==7.1.0
kiwisolver==1.5.1
libusb-package==1.0.26.3
matplotlib==3.11.2
numpy==2.5.4
packaging==26.3
pandas==3.1.0
pillow==13.0.0
platformdirs==4.14.0
psutil==7.2.2
Pygments==2.21.0
pyparsing==3.3.3
pyperclip==1.11.0
pyqtdarktheme==2.1.0
pyqtgraph==0.14.0
pyserial==3.5
PySide6==6.8.3
PySide6_Addons==6.8.3
PySide6_Essentials==6.8.3
python-dateutil==3.0.0
pyusb==1.3.1
PyYAML==6.0.3
QtAwesome==1.4.2
QtPy==2.4.3
requests==2.34.2
rich==12.6.0
scipy==1.18.1
shiboken6==6.8.3
six==1.17.0
soupsieve==3.0.4
textual==0.1.18
typing_extensions==4.16.0
tzdata==2026.6
urllib3==2.8.0
xlsxwriter==3.3.1
Traceback
Traceback (most recent call last):
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool\app\new\backend_model.py”, line 96, in connect_client
self.client = client_factory()
^^^^^^^^^^^^^^^^
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool\a121_core\communication\client.py”, line 51, in open
return super().open(
^^^^^^^^^^^^^
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool_core\communication\client.py”, line 88, in open
return subclass.open( # type: ignore[no-any-return, attr-defined]
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool\a121_core\communication\exploration_client.py”, line 98, in open
return cls(client_info=client_info)
^^^^^^^^^^^^^^^^^^^^^^^^^^^^
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool\a121_core\communication\exploration_client.py”, line 124, in init
self._server_info = self._retrieve_server_info()
^^^^^^^^^^^^^^^^^^^^^^^^^^^^
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool\a121_core\communication\exploration_client.py”, line 149, in _retrieve_server_info
system_info_response = self._server_stream.wait_for_message(messages.SystemInfoResponse)
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool_core\communication\message_stream.py”, line 67, in wait_for_message
for msg in self._stream:
^^^^^^^^^^^^
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool_core\communication\message_stream.py”, line 95, in _get_stream
self._error_callback(e)
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool\a121_core\communication\exploration_client.py”, line 145, in _close_before_reraise
raise exception
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool_core\communication\message_stream.py”, line 93, in _get_stream
header_in_bytes = self._link.recv_until(self.protocol.end_sequence)
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool_core\communication\links\serial_link.py”, line 159, in recv_until
raise LinkError(msg)
acconeer.exptool._core.communication.links.buffered_link.LinkError: recv timeout
During handling of the above exception, another exception occurred:
Traceback (most recent call last):
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool\app\new\backend_backend.py”, line 235, in process_generator
model.execute_task(task)
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool\app\new\backend_model.py”, line 60, in execute_task
builtin_task(**kwargs)
File “C:\Users\C\AppData\Local\uv\cache\archive-v0\LL5mImRW-3mWMlkm\Lib\site-packages\acconeer\exptool\app\new\backend_model.py”, line 102, in connect_client
raise HandledException(msg)
acconeer.exptool.app.new._exceptions.HandledException: Failed to connect:
recv timeout