ZED-X20P – BeiDou B1 and B2 Signals Tracked in u-center 2 but Missing from Raw Data Recording

Hi,

I am using the u-blox ZED-X20P GNSS module.

When connected to the module through u-center 2, I can see that the BeiDou L1 and L2 signals are being tracked.

However, when I record the raw GNSS data, measurements for these particular BeiDou frequencies are missing from the recorded data. Other GNSS constellations and the other BeiDou frequencies are being recorded correctly.

Is there any specific receiver configuration, message configuration, or signal-enable setting required to ensure that the BeiDou L1 and L2 measurements are included in the raw data recording?

Has anyone encountered a similar issue with the ZED-X20P?

Any suggestions would be appreciated.

Thanks!

@PaulZC

Hi Abhishek (@Abhishek_Kailash ),

How are you recording the RXM-RAWX messages? Through u-center? Or through our Arduino Library?

Which firmware version is your X20P running?

Best wishes,
Paul

Through u-center 2 only. HPG 2.02 firmware is installed

OK. Thank you.

I suggest upgrading to HPG 2.11 just in case there have been any changes to the BeiDou RAWX reporting.

Things to try:

I suggest asking your question on the u-blox portal. Someone there may know the answer.

Please check the setting of CFG-BDS-D1D2_NAVDATA. It should be set to zero (“ALL”)

I hope this helps,
Paul

Adding a link to the u-blox portal: