Hi all;
As the title says, I am running 2g continuous servos (yes 2 gram servos) for my micro project, these will later be switched out for smaller 1.7g servos as they have a smaller footprint without getting into custom made servos. I am also currently running these off of an Arduino Nano and a 12V stepped down to 5V via a converter that I know is good (through a different project using Car voltage) this will also be switched out later for a 5V mini battery.
The issue that I am running into is that after a few moves (maybe 5) of the servos, they start to no longer fully move back to their final/initial point in space which is at 200° & 0° respectively. This is without any real load on them, one of them is moving a tiny metal wire which moves a pivot point, the second is pulling an elastic string against the opposing string of the same force value.
Both servos are sent a signal separately as to not have any mixed values, and they’re also receiving power directly from the voltage converter
So my I would like to know your guys thoughts on the matter as it has caused a road block in my project which I cannot get passed with my limited knowledge.