Hi.
In the end, I want a 12v PWM signal to drive a Solid State Relay (SSR) , which will drive a 12v pump motor and or a 12v fan. Giving the pump or fan a variable speed depending on the signal.
But Arduino zero (fast 48MHz and 10bit) only outputs 3.3v PWM signal.
Someone suggested to look at a logic level converter but the way I understood it was that it only deals with HIGH and LOW?
Is there a product that can do what I want?..
Do I indeed NEED a 12v PWM signal to operate a 12v device? Will a 3.3v PWM at 100% duty cycle run the 12v motor at full speed???..