Hello Sparkfunners,
Had an idea for a linear LED display project that
would turn on 320 LEDs one at a time then
turn them all of at once and then relight
them one at a time using an Arduino Uno
as a controller.
Started with the Max7219 but the IC
is designed to operate an 8x8 matrix
or a seven segment display and the
breakout to a linear geometry was
a rat’s nest nightmare.
Then the SparkFun 74H595 Shift
Register Breakout board (BOB-10680)
was fgound which provided a more linear array.
The article that was the catalyst
http://bildr.org/2011/08/74hc595-breakout-arduino/
which talks about “1000 of these chained together”.
But the article was misunderstood.
The daisy-chained Sparkfun Breakout boards
can control hundreds of LEDs
but it can only turn on a dozen
or so at one time.
The specs on the 3mm LEDs say they draw
20mA per diode.
The spec sheet on the Arduino lists
the ampereage output for the 3 volt
supply at 50 mA but does not list amps
for the 5v supply. But some digging
around on the forum reveals that
a safe limit is about 450 mA.
The 3mm LEDs used in the project
draw 20mA. So if my math is correct
I can have 22 LEDs on at a time.
Hoping to decrease the amps
required to control the LEDs
and increase the number of diodes
that could be controlled the idea of having
the breakout board control transistors
that supply hight voltage/amperage
was envisioned and design for such
an araangement is displayed herewith.
If the datatsheets for the transistors
is read correctly the current needed
to turn on the transistor is
2N3904 .1 mA 1v
BC108 2 mA 5v
BC182 2 mA 5v
BC548 2 mA 5v
I beleievev that with any of these transistors R1
could be fairly low like 100 ohms.
Is there a transistor that takes
less current to be come saturated?
Assuming these ideas hold true then
the design of the circuit controlled by the
breakout boards is the focus.
Again the LEDs draw 20mA per unit.
If the the display is 320 LEDS that
is 6400 mA or 6.4 amps. Is that right?
I see some power supplies up around 5 amps
but not any at 6 amps.
What is the method for calculating R2
and the voltage and amperage of the
LED power supply?
Thanks.
Allen Pitts, Dallas Texas