Has anybody implemented the 4-bit MCI SD card interface on LPC23xx or LPC24xx? Or on any processor.
Is there any example code out there?
There’s quite a bit of info in the LPC23 manuals but not really enough to put together a practical system. A while ago Sandisk had a pretty good .pdf about this, which now seems to be censored right where the good stuff starts. Should have saved it then.
denial:
Try the MMC standard. The latest version is freely available at the mmca.org website.
Thanks, that looks to pretty thorough. Frankly though, I just gave up and will go with the old SPI interface this time around, which I have found still works OK with at least the SanDisk Micro_SD 2GB. However it's a little scary to think that SPI is "optional" in the Micro_SD spec itself, and I presume also in the new high capacity cards. Sooner or later we're going to have to crack the 4-bit interface.