here is script from the GNUARM/Eclipse tutorial
// 				Setting the Phased Lock Loop (PLL)
	//               ----------------------------------
	//
	// Olimex LPC-P2106 has a 14.7456 mhz crystal
	//
	// We'd like the LPC2106 to run at 53.2368 mhz (has to be an even multiple of crystal)
	// 
	// According to the Philips LPC2106 manual:   M = cclk / Fosc	where:	M    = PLL multiplier (bits 0-4 of PLLCFG)
	//																		cclk = 53236800 hz
	//																		Fosc = 14745600 hz
	//
	// Solving:	M = 53236800 / 14745600 = 3.6103515625
	//			M = 4 (round up)
	//
	//			Note: M - 1 must be entered into bits 0-4 of PLLCFG (assign 3 to these bits)
	//
	//
	// The Current Controlled Oscilator (CCO) must operate in the range 156 mhz to 320 mhz
	//
	// According to the Philips LPC2106 manual:	Fcco = cclk * 2 * P    where:	Fcco = CCO frequency 
	//																			cclk = 53236800 hz
	//																			P = PLL divisor (bits 5-6 of PLLCFG)
	//
	// Solving:	Fcco = 53236800 * 2 * P
	//			P = 2  (trial value)
	//			Fcco = 53236800 * 2 * 2
	//			Fcc0 = 212947200 hz    (good choice for P since it's within the 156 mhz to 320 mhz range
	//
I dont understand how we can get the LPC2106 running at 53.2368 mhz as it is not even multiple of 14.7456 mhz. with the PLLCFG set to 0x23, shouldnt the LPC2106 run at 58.9824 mhz.
pls help