Vraz:
I currently use API mode 2
Am going to get one of the Microchip modules and see if I can get it talking to the XBee. That would put me in good shape for the long term.
Trying Microchip ↔ XBee just for the heck of it? Why not just use one or the other? Digi/XBee is unlikely to be discontinued any time soon.
I use the API mode that doesn’t use byte stuffing/escape- can’t recall if that is mode 1 or 2.
Re Microchip… Quote from their web page. It’s very true, no matter the vendor.
Alternative Protocols
Due to the fact that the ZigBee protocol has grown too large and complex for many applications, a large percentage of the market for IEEE 802.15.4 wireless Personal Area Networking is likely to use alternative, proprietary protocols, such as the MiWi protocol. Additionally, ZigBee protocol certification is costly and cumbersome for small- and medium-size companies. Microchip’s MiWi protocol provides a simpler, lower-cost solution for customers who do not need interoperability but still want to use robust IEEE 802.15.4 radios.
IEEE 802.15.4 is public, open. ZigBee is proprietary to, licensed by that alliance. Other popular network layer protocols for 802.15.4 include ISA 100.11a and 6LoWPAN, however these are complex and specialized. Also, 802.15.5 (new) is an open standard for meshing with 802.15.4.
Microchip is a chip vendor, not an OEM module vendor as is Digi who uses Freescale (series 1) and Ember (Series 2). The OEM modules (Digi, Jennic, others, are type certified (legal) for use in various countries), meaning the OEM need not bear this cost and delay. The chip vendors all have eval/dev boards, but these aren’t viable as OEM modules.
Looks like Microchip’s MiWi P2P is the same as XBee when configured for P2P using AT setup commands (one time).
My understanding is that 80% or more of all vendor’s 802.15.4 modules sold are without ZigBee. The ZigBee gang was too late to capture the beginning of the smart-grid movement and they were too late for Home Automation (Z-Wave got that). But finally, Utility industry companies are trying to force their meter vendors to comply with standards instead of being proprietary as they have been to date, in wireless, mostly 900MHz.
Beware though, the dependencies; example: Digi XBee series 1 is not ZigBee by intent whereas Series 2, being based on Ember’s chip, must load up with ZigBee, as I understand, by contract agreement.
Anyone know of a type certified OEM module based on Microchip’s 1mW or 100mW chips? These are relatively new.