I recently bought the SparkFun 9DoF Razor IMU M0 which combines a SAMD21 microprocessor with an MPU-9250 9DoF (nine degrees of freedom). My propose with this equipment was to record on the µSD card data from the 3-axial accelerometer. The data needs to have a 200Hz (or more) sample rate. According with your description the sample rate of the accelerometer and gyroscope can reach 1kHz. Therefore, I was expencting the equipment to easily fulfill my needs. However, that is not happenig at all. I only can reach a maximum 100Hz sample rate. I’m using a Lexar 633x µSD card.
So, I would like to know if there is any limitation for data record with sample rate above 100Hz? This limitation is related with the µSD card? Or should the equipment allow me to reach a higher sample rate? What can I do to reach it?