First, I posted this in another forum as well, not sure which is most appropriate.
That post can be found here viewtopic.php?f=74&t=59326
Here’s the trouble: Connecting an LPS28DFW to a DEV16832, fresh out of the box, the startup reads:
Please ensure the SD card is formatted correctly using https://www.sdcard.org/downloads/formatter/
Config file read failed: SD offline
Artemis OpenLog v2.4
SD card offline
Datalogging offline
Serial logging offline
IMU online
Identifying Qwiic Muxes...
Identifying Qwiic Devices...
Known I2C address but device failed identification at address 0x5C
Unknown device at address (0x7E)
Autodetect complete
Device config file read failed: SD offline
Content-Type: text/csv
I have reset, rescanned, tried with SD card attached, 1300 mAh battery after charging overnight, no change.