When I try to use the ADIN1110 examples, with Arduino IDE 2.3.2
and I connect the ADIN1110 board on the SparkFun Main Board Single by using an ESP32 MicroMod Board, during upload the code I get alltimes an error:
Without connecting the ADIN1110 PCBA the upload works, look like some missmatch of the SPI or I2C communication to the Flash … → ADIN1110 PCBA disturbe the ESP32 after Power during the upload?
Chip is ESP32-D0WDQ6-V3 (revision v3.1)
Features: WiFi, BT, Dual Core, 240MHz, VRef calibration in efuse, Coding Scheme None
Crystal is 40MHz
MAC: 34:98:7a:4c:be:d8
Uploading stub…
Running stub…
Stub running…
Changing baud rate to 921600
Changed.
WARNING: Failed to communicate with the flash chip, read/write operations will fail. Try checking the chip connections or removing any other hardware connected to IOs.
Configuring flash size…
o execute script ‘esptool’ due to unhandled exception!
Failed uploading: uploading error: exit status 1
some news: (update 2024-08-15 11:30) → Remove R22
now the upload with the connected ADIN1110 PCBA is working,
==> but the SPE comunication is not working at all, there is no LINK LED, no LDC Display Infos …