Greetings all and happy Thanksgiving!
Please, I am trying to write a code to control the gripper closing force or angle according to a reading from a sensor ( I am not sure if only one sensor needed or two)
so the gripper servo will respond and go to the best closing angle which is enough to:
Hold tight the object
Lift the object for two seconds or so
put back the object
Release object
The serial monitor will display Force applied and adjusted gripper Angle continuously while dealing with each object
The gripper will expect another object ( I am trying to use three different sizes or weights) to gripp, hold and lift and put back so in this case the gripper will adjust to new angle or pressure. My gripper works between ~ 45 degrees (full open) to ~ 110 degrees (full close)
Please i need help with such a code. I could get a reading from sensors every time i press on them but i could not so far able to code the gripper adjustment around each object
Here is my test code:
#include <Servo.h>
Servo s1;
Servo s2;
int pos;
int fsr = 15; // pin for sensor and 10k resistor
int force; // analog reading
void setup()
{
Serial.begin(9600);
s1.attach(8);
s2.attach(9);
}
void loop()
{
s2.write(45); //start gripper open
delay(1000);
s2.write(100);
force = analogRead(fsr); // FSR reading
Serial.print("FSR reading = ");
Serial.println(force); // display fsr value when gripper close
pos = map(force, 0, 1023, 45, 100); // relates force reading to degrees of gripper servo position
Serial.print("Gripper Angle = ");
Serial.println(pos); // gripper angle reading from pos
delay(300);
if(force < 1 ){
s2.write (90);
if(force = 10){
s2.write(85);
if(force >18){
s2.write(75);
}
}
}
s2.write(pos); // go to pos
delay(250); // Delay 250 milliseconds
s1.write(25); //the object will be lifted
delay (3000);
s1.write(0); // put down object
delay (1000);
}
Electronics:
I have one sensor attached to each gripper finger.
One servo for gripper
One servo to lift arm
Arduino Mega 2560 microcontroller
Interlink Electronics 0.5" Circular FSR
Interlink Electronics 1.5" Square FSR
Thank you so much. Your help will make much difference!