I just seem to be full of problems with this project…
Working with a 3-axis accelerometer, wiring x, y, and z into the 1219’s pins Ain0, Ain1, and Ain2. Pull-up resistors are in place at Ain0, Ain1, and Ain2.
All of my ADC “reads” seem to only be seeing Ain1.
It’s probably a simple mistake… Please help?
#include <SparkFun_ADS1219.h> // Click here to get the library: http://librarymanager/All#SparkFun_ADS1219
SfeADS1219ArdI2C myADC;
void setup() {
// put your setup code here, to run once:
delay(1000); // Allow time for the microcontroller to start up
Serial.begin(115200); // Begin the Serial console
while (!Serial)
{
delay(100); // Wait for the user to open the Serial Monitor
}
Wire.begin(); // Begin the I2C bus
// Initialize ADC - this also performs a soft reset
while (myADC.begin() == false)
{
Serial.println("ADC failed to begin. Please check your wiring! Retrying...");
delay(1000);
}
// Configure the input multiplexer. Options are:
// ADS1219_CONFIG_MUX_DIFF_P0_N1 (Default)
// ADS1219_CONFIG_MUX_DIFF_P2_N3
// ADS1219_CONFIG_MUX_DIFF_P1_N2
// ADS1219_CONFIG_MUX_SINGLE_0
// ADS1219_CONFIG_MUX_SINGLE_1
// ADS1219_CONFIG_MUX_SINGLE_2
// ADS1219_CONFIG_MUX_SINGLE_3
// ADS1219_CONFIG_MUX_SHORTED
//myADC.setInputMultiplexer(ADS1219_CONFIG_MUX_SINGLE_0); // Read the voltage between AIN0 and GND
Serial.println(“ADC initialized”);
Serial.println(“Reading the voltage through the input multiplexer”);
}
void loop() {
myADC.startSync(); // Start a single-shot conversion.
while (myADC.dataReady() == false) // Check if the conversion is complete. This will return true if data is ready.
{
delay(10); // The conversion is not complete. Wait a little to avoid pounding the I2C bus.
}
myADC.setInputMultiplexer(ADS1219_CONFIG_MUX_SINGLE_0); // Read the voltage between AIN0 and GND
myADC.readConversion(); // Read the conversion result from the ADC. Store it internally.
float milliVolts0 = myADC.getConversionMillivolts(); // Convert to millivolts.
Serial.print("ADC voltage Ain0 (mV): ");
Serial.println(milliVolts0, 6); // Print milliVolts with 6 decimal places
myADC.setInputMultiplexer(ADS1219_CONFIG_MUX_SINGLE_1);
myADC.readConversion(); // Read the conversion result from the ADC. Store it internally.
float milliVolts1 = myADC.getConversionMillivolts(); // Convert to millivolts.
Serial.print("ADC voltage Ain1 (mV): ");
Serial.println(milliVolts1, 6); // Print milliVolts with 6 decimal places
myADC.setInputMultiplexer(ADS1219_CONFIG_MUX_SINGLE_2); // Read the voltage between AIN0 and GND
myADC.readConversion(); // Read the conversion result from the ADC. Store it internally.
float milliVolts2 = myADC.getConversionMillivolts(); // Convert to millivolts.
Serial.print("ADC voltage Ain2 (mV): ");
Serial.println(milliVolts2, 6); // Print milliVolts with 6 decimal places
delay(250);
}
As it sits, the accelerometer is tilted on the y axis, so Ain1 should be ~465, and Ain0 and Ain2 should be ~388.