After working on this hobby project for almost a year, I am so proud to finally say that it’s complete. Fintic, the name of this project, is a desk size LED matrix ticker that could display all kinds of information. From stocks, crypto, forex prices, to news, weather, sports and even custom uploaded images, GIFs and messages, all controlled via a web server! I plan to add even more features in the future.
The hardware consists of two 64x32 P3 LED Matrix panels, a Raspberry Pi 3 A+, the Adafruit RGB Matrix bonnet, a 5V 14A power supply and a custom 3D printed frame to fit everything inside!
The code was written in both Python and C++, and is primarily based on the Hzeller’s RPI RGB Matrix library. Check out some examples of the ticker in work below ![]()
Custom uploaded images, GIFs, messages:
https://i.imgur.com/Np2WLGO.png
Stocks, crypto, forex:
https://i.imgur.com/9EioYkj.png
News:
Weather:
Sports:
This project was highly inspired by my time in NYC. Seeing all the scrolling tickers and LED billboards in Times Square, and Wall Street was so exciting and I wanted to recreate that atmosphere in a home environment. With that said, I have the ticker turned on pretty much everyday now haha! So what do you guys think? ![]()