I have just gotten a LPC-H2138 and its the 1st time using an ARM I use IAR Embedded Workshop.
1st I Downloaded the blinky source code from olimex.
2nd I Downloaded the lpc2000 flash utility from philips.
3rd I turn on both switchs and removed the jumper so that jtag port would be disabled
4th In IAR I changed from debug to release
5th I changed under the Linker from elf to intel extended.
6th I clean and rebuild all
7th I open LPC2000 utility goto buffer then flash buffer load the file then click vector cal and save the file and close the window.
8th I click the … and select the file I just saved
9th I click Upload To Flash and it programs the lpc
10th I click Compare Flash and it comares and finds a match.
But the code still won’t run for somereason I dunno why
I have a check next to Use DTR/RTS for reset and bootloader selectrion also I have a check next to Execute Code after Upload. I have tried Unchecking both and reflashing and still not had any luck.
Does any one have a compiled and ready to go HEX for the blinky code that I can try and load to see if maybe its something to do with IAR?
Or if someone else has encountered the same problem a little help would be very appricated.
Thanx,
Cranky