Version v2.1 of Armaide, the LPC2000 Oberon-07 development system was released this week. New features include:
Local dynamic arrays - these allow you to resize arrays of any type at runtime with no need for a garbage collector and no risk of memory leaks or fragmentation.
Resource file handling for large quantities of constant data (fonts, bitmaps etc.) - the files are appended to the executable at link time and accessed like an array using functions from the new library module ResData.
‘What’s New in v2.1’ is a summary of all the new features. It can be downloaded from:
http://www.cfbsoftware.com/armaide/WhatsNew.htm
For more detailed information download the document ‘Oberon for LPC2000 Microcontrollers’ from: