I have the module on the Sparkfun $29.95 breakout board connected to the PC serial port via MAX2323.
Everything is fine, i can send and receive commands to the module.
But as soon as ist connects or tries to connect to a GSM-network, the modules shuts down itself.
So, everything is cool, until i put in a SIM card and enter the PIN.
Or, if i unplug the antenna, I can reach the simcard, the module stays on, because it gets no network.
But, as soon as unlocked SIM AND antenna is connected, so the module could connect to a network unhindered - arbitrary self-switchoff. ![]()
Current firmware version is 07.02.403
I already changed to a former firmware 07.02.402 - same problem.
Has anyone experienced this behavior as well?
How can I be helped?