Hi,
I’m having some issues with my 5 Volt Arduino. And it’s quite odd. The following sketch:
int count;
void setup() {
  Serial.begin(38400);
  count = 1;
}
void loop() {
  Serial.println(count);
  count++;
  digitalWrite(13, HIGH);
  delay(500);
  digitalWrite(13, LOW);
  delay(500);
}
It works great on my 3.3 Volt Arduino. But my 5 volt one only spits giberish out the serial port:
%ó¥Eø¥<ó¥óeEó%EóKFû%Fó¥Dù¥"ø¥ó¥:ó¥ó[Dû¥Eø%Eó¥>ó¥ó 8
I’ve double checked the baud rate on the serial monitor. I’ve also tried different baud rates in the sketch and the monitor. It does not correct the problem. I thought that maybe I broke my microcontroller or my FTDI. So I purchased new ones, and I am still having this problem. I also tried running this on a different computer. No such luck. I don’t get it. The serial port must be working because it loads sketches on without a problem. And it works fine with my 3.3 volt Arduino and FTDI connector. Any suggestions?
- Chris