So I have what I feel like is a very newbie question here.
I have a Arduino with a Motor controller that can drive up to 24 volts and pull 30 amps. I can get my motor working without any issue. My question is when I place the motor under load it of course as we would expect pulls a lot of amps… it actually can pull way more then my board can handle.
My question is as follows if I let the motor pull as much power as it wants (assuming my board does not burn up) I will drain my battery insanely fast. Is there any way to limit or cap the amount of draw the motor is allowed to take from my board / power supply. I would rather shut the motor down when it’s load is pulling more then 20 amps then continue to draw more power.
If it helps under normal operations I am able to run at about 10 - 15 amps. When I get stuck on carpet, a crack in the pavement etc… things I did not detect with my range sensors the wheels seems to get “stuck” and it draws more and more current.