With a rechargeable lithium ion batteries 9v, Can I connect it directly to the arduino pro mini? Or do I have to use a voltage regulator?
According to SparkFun’s site the two types of pro-minis work up to 12v on the raw input.
Here’s the datasheet for the onboard regulators: http://www.micrel.com/_PDF/mic5205.pdf
Remember to take thermal dissipation into consideration… Or it may get rather toasty. ![]()
it depends on how much stuff will be powered through the regulator on the pro mini.
Im running a pro mini with 12V into RAW - powering the pro mini and a couple other ics that also use the pro mini regulator. The regulator is warm and i keep an eye on it. Im using the pro mini to send out logic to a bunch of other components that are directly on the 12v line. i think i would rethink this setup if i added even one LED to the mix. There are some nice switching 5V regulators available.
it all seems to be working fine.