With my current project, I am planning on using an [Arduino Teensy (the smallest board they have) to control two 12V solenoids. I’m planning on running the solenoids off of a 14.8v lipo battery, so I believe I need to use a MOSFET for each solenoid so I don’t fry my board.
In the wiring diagram I found online for this (pictured below), the MOSFET gets soldered to the [Arduino’s ground, but since the ground is shared with the solenoid’s ground, wouldn’t this send 14.8 volts directly into my Teensy, frying it? I was hoping to use a small 3.4V lipo for the Teensy, but I’m worried about frying the Teensy from the massive brick being used to power the solenoids. Any suggestions or answers are greatly appreciated!](Arduino UNO Price in Pakistan | w11stop.com)](Arduino UNO Price in Pakistan | w11stop.com)