Arduino Theremin Help

hello all,

I am currently working on the project from this site:

<LINK_TEXT text="
http://interface.khm.de/index.php/lab/ … ng-device/">
http://interface.khm.de/index.php/lab/interfaces-advanced/theremin-as-a-capacitive-sensing-device/</LINK_TEXT>

If you scroll down you will find a video of the theremin. You will notice a wobbly effect. The hand clearly changes the frequency, but I found the same wobbled effect of the notes. They seem to be constantly changing. So even when my hand is not there, the frequency changes.

I thought that it would be better if there was a single note/frequency. I am trying to demonstrate how a theremin works. Thus, is it possible to get rid of this wobbled effect and get a single note. I have no clue why that effect is there in the first place.

My second question is: I built his circuit on a breadboard and hooked it all up. My only problem is that the sound is much quieter than what he has. Is there any way for me to increase my volume.

Thanks.

There is no need to create multiple threads. This confuses communication. Please choose one of the threads and close the other.

The other thread for reference:

https://forum.sparkfun.com/viewtopic.php?f=42&t=40362

I can’t seem to play the video on that blog, not with IE 10 or Chrome. Hard to say what could be the cause without the schematic, or the code of the arduino. As the latter is supposed to be able to sense the feedback on the lc oscillator.

Sorry about the dual threads.

The video works well on firefox. I don’t know why it doesn’t work on chrome or IE.

The schematic and Arduino code are on the link.

Here is a link for the schematic as well: http://interface.khm.de/wp-content/uplo … ch_web.jpg

The circuit is using the gates as amplifiers to increase the sensitivity. The problem maybe the circuit is picking up electrical interference from appliances, AC power wiring, radio stations, and whatever electronics in the vicinity. The circuit is responding to the noise it is picking up. This is cause of the changes without a hand nearby.