1.- The “sketch not working” phrase is just to denote a problem, did not mean the original sketch was not working, if you read the whole text, I also ask: “What am I missing”??? You obviously did not read that part, but yes, I know it is not the sketch, so wasted words there, codlink.
2.- Here is the sketch that everybody has, since like I said, it is in the list of sample sketches that come with the IDE:
/*
WiFi Web Server
A simple web server that shows the value of the analog input pins.
using a WiFi shield.
This example is written for a network using WPA encryption. For
WEP or WPA, change the Wifi.begin() call accordingly.
Circuit:
created 13 July 2010
by dlf (Metodo2 srl)
modified 31 May 2012
by Tom Igoe
*/
#include <SPI.h>
#include <WiFi.h>
char ssid = “yourNetwork”; // your network SSID (name)
char pass = “secretPassword”; // your network password
int keyIndex = 0; // your network key Index number (needed only for WEP)
int status = WL_IDLE_STATUS;
WiFiServer server(80);
void setup() {
//Initialize serial and wait for port to open:
Serial.begin(9600);
while (!Serial) {
; // wait for serial port to connect. Needed for Leonardo only
}
// check for the presence of the shield:
if (WiFi.status() == WL_NO_SHIELD) {
Serial.println(“WiFi shield not present”);
// don’t continue:
while (true);
}
String fv = WiFi.firmwareVersion();
if ( fv != “1.1.0” )
Serial.println(“Please upgrade the firmware”);
// attempt to connect to Wifi network:
while ( status != WL_CONNECTED) {
Serial.print("Attempting to connect to SSID: ");
Serial.println(ssid);
// Connect to WPA/WPA2 network. Change this line if using open or WEP network:
status = WiFi.begin(ssid, pass);
// wait 10 seconds for connection:
delay(10000);
}
server.begin();
// you’re connected now, so print out the status:
printWifiStatus();
}
void loop() {
// listen for incoming clients
WiFiClient client = server.available();
if (client) {
Serial.println(“new client”);
// an http request ends with a blank line
boolean currentLineIsBlank = true;
while (client.connected()) {
if (client.available()) {
char c = client.read();
Serial.write(c);
// if you’ve gotten to the end of the line (received a newline
// character) and the line is blank, the http request has ended,
// so you can send a reply
if (c == ‘\n’ && currentLineIsBlank) {
// send a standard http response header
client.println(“HTTP/1.1 200 OK”);
client.println(“Content-Type: text/html”);
client.println(“Connection: close”); // the connection will be closed after completion of the response
client.println(“Refresh: 5”); // refresh the page automatically every 5 sec
client.println();
client.println(“”);
client.println(“”);
// output the value of each analog input pin
for (int analogChannel = 0; analogChannel < 6; analogChannel++) {
int sensorReading = analogRead(analogChannel);
client.print("analog input ");
client.print(analogChannel);
client.print(" is ");
client.print(sensorReading);
client.println("
");
}
client.println(“”);
break;
}
if (c == ‘\n’) {
// you’re starting a new line
currentLineIsBlank = true;
}
else if (c != ‘\r’) {
// you’ve gotten a character on the current line
currentLineIsBlank = false;
}
}
}
// give the web browser time to receive the data
delay(1);
// close the connection:
client.stop();
Serial.println(“client disonnected”);
}
}
void printWifiStatus() {
// print the SSID of the network you’re attached to:
Serial.print("SSID: ");
Serial.println(WiFi.SSID());
// print your WiFi shield’s IP address:
IPAddress ip = WiFi.localIP();
Serial.print("IP Address: ");
Serial.println(ip);
// print the received signal strength:
long rssi = WiFi.RSSI();
Serial.print(“signal strength (RSSI):”);
Serial.print(rssi);
Serial.println(" dBm");
}
3.- If you researched and found a sketch using the sparkfun’s WiFi shield as server, then that’s all I need. I have googled it in many ways, but I guess I am not using the right words, maybe.
4.- By the way… I know I need to use the SFE library and methods. I just don’t know how what the server related objects and methos are. I also know I am doing something wrong, otherwise I wouldn’t be asking… Don’t you think, codelink?
5.-Hey… If my questions are bothering somebody, just let me know, I guess this is not the only place I can ask questions, without offending anybody.