Arduino WiFi server / client

Is it possible to make the arduion act like a server and as a client in the same time… not in the same time, but to do them both.

Server - to listen for incomming clients, and save the data into a file

this part works.

Client - to connect to a webpage and send some data (get variables)

!#@!@U

the client part is where I have problems… It connects to the page, it prints the content of it in serial, but then it hangs, it won’t “see” any new “clients” when i try to access it via browser.

I’ll provide the code too, maybe you can tell me what’s wrong.

it triggers the requestPage function if there’s a blabla in url

#include <SPI.h>
#include <WiFi.h>


char ssid[] = "PinkLink";      // your network SSID (name) 
char pass[] = "unu1doi2trei3";   // your network password

int status = WL_IDLE_STATUS;

String currentLine = "";

WiFiServer server(80);
WiFiClient client;
void setup() {
  //Initialize serial and wait for port to open:
  Serial.begin(115200); 
  while (!Serial) {
    ; // wait for serial port to connect. Needed for Leonardo only
  }
  
  // check for the presence of the shield:
  if (WiFi.status() == WL_NO_SHIELD) {
    Serial.println("WiFi shield not present"); 
    // don't continue:
    while(true);
  } 
  
  // attempt to connect to Wifi network:
  while ( status != WL_CONNECTED) { 
    Serial.print("Attempting to connect to SSID: ");
    Serial.println(ssid);
    // Connect to WPA/WPA2 network. Change this line if using open or WEP network:    
    status = WiFi.begin(ssid, pass);

    // wait 10 seconds for connection:
    delay(10000);
  } 
  server.begin();
  // you're connected now, so print out the status:
  printWifiStatus();
  currentLine.reserve(256);
}

void loop() {
    asteaptaClient();
}

void requestPage() {
  /*  
  char serverName[] = "puiucristian.com";
    if (client.connect(serverName, 80)) {
      client.println("GET /bu.php HTTP/1.1");
      client.println("Host: puiucristian.com");
      client.println("Connection: close");
      client.println();
      delay(1);
    }
    */
  }

void asteaptaClient() {
    // listen for incoming clients
    client = server.available();
    
  if (client) {
    Serial.println("new client");
    // an http request ends with a blank line
    boolean currentLineIsBlank = true;
    while (client.connected()) {
      if (client.available()) {
        char c = client.read();
        currentLine += c;
        // if you've gotten to the end of the line (received a newline
        // character) and the line is blank, the http request has ended,
        // so you can send a reply
        if (c == '\n' && currentLineIsBlank) {
          // send a standard http response header
          client.println("HTTP/1.1 200 OK");
          client.println("Content-Type: text/html");
          client.println("Connection: close");  // the connection will be closed after completion of the response
          client.println();
          client.println("<!DOCTYPE HTML>");
          client.println("<html>");
          // output the value of each analog input pin
          for (int analogChannel = 0; analogChannel < 6; analogChannel++) {
            int sensorReading = analogRead(analogChannel);
            client.print("analog input ");
            client.print(analogChannel);
            client.print(" is ");
            client.print(sensorReading);
            client.println("
");       
          }
          client.println("</html>");
           break;
        }
        if (c == '\n') {
          // you're starting a new line
          currentLineIsBlank = true;
        } 
        else if (c != '\r') {
          // you've gotten a character on the current line
          currentLineIsBlank = false;
        }
      }
    }
    // give the web browser time to receive the data
    delay(1);
    
    // close the connection:
    client.stop();
    Serial.println("client disonnected");
    //Serial.print(currentLine);
    if(currentLine.indexOf("blabla") != -1) {
       requestPage(); 
    }
    currentLine= "";
  }
}

void printWifiStatus() {
  // print the SSID of the network you're attached to:
  Serial.print("SSID: ");
  Serial.println(WiFi.SSID());

  // print your WiFi shield's IP address:
  IPAddress ip = WiFi.localIP();
  Serial.print("IP Address: ");
  Serial.println(ip);

  // print the received signal strength:
  long rssi = WiFi.RSSI();
  Serial.print("signal strength (RSSI):");
  Serial.print(rssi);
  Serial.println(" dBm");
}