Hey guys, i’m having a problem connecting to the internet using my CC3000 module. Now, I’ve followed the schematic on this link :[Schematic+code, and i used the library and WebClient example provided on the site.
Note, i don’t have a level shifter so i used a voltage divider (3x10kOhhm resistor when i’m sending from Arduino to Wifi, so it’s 5V(arduino)->Voltage divider->3.3(Wifi module), and a circuit with a Si Diode and a 10k Resistor to up the voltage level from 3.3V to 5V (i’ll provide a picture.). The problem I’m having is that the Arduino doesn’t pass the initialize faze and just gets stuck. This is really urgent so i would love if someone could give me a hand as fast as possible, thank you.
I need some help with this since i’m lost on what more can i change to try. Thanks in advance, pictures included below.
https://scontent.fbud2-1.fna.fbcdn.net/ … e=59D078A7
https://scontent.fbud2-1.fna.fbcdn.net/ … e=59D0591F](https://learn.sparkfun.com/tutorials/cc3000-hookup-guide#cc3000-library-installation)