ARM development software

Hi,

I’m a ARM newbie.

What is the “state of the art” free ARM development software.

I often read about WINARM. On the internet I found an old

version from 2006. Is WINARM obsolete?

Please give me some advices.

Many thanks,

Hello,

You may also try YAGARTO or CodeSourcery toolchains, both include more recent compiler versions and utilities.

www.yagarto.de

www.codesourcery.com

Both can be used under Eclipse to form a complete development environment (Eclipse+CDT+Zylin plugin+OpenOCD).

The setup of the thing is not so easy but it is a very complete and powerful development environment,

regards,

Giovanni

i use keil mdk3.70 demo: 32k code limitation, though enough for what i do.

Keil and IAR have 32KB free versions, non-commercial use.

Much, much better than GCC/Rowley, YAGARTO/WINARM in terms of your productivity and eliminating the need to focus on your tools rather than your project.

I’m pleased with IAR, having tried them all.

Rowley CrossWorks for ARM has an excellent IDE and debugger/simulator, and support is very good.

Leon

leon:

i took a look at your website and was particularly interested in the minimalistic dev board you have there.

as I am new to ARM/LPC, I would love to get your help on a few questions:

  1. jtag/ulink/wiggler/etc.: what is the purpose to have those “devices”? why do you need to have a hardware debug feature? if anything, i am used to debug my program in ide and then flash it to the mcu and let it run. what advantages does having a jtag for example bring?

  2. what are the ways to flash my program onto the mcu? you mentioned the bootloader approach: how does it work? it seems to be only available to (certain?) lpc chips. seems the mcu already has icp/isp pins all you need is a rs232 and the right program - maybe you need to reverse the rst line.

  3. my intended mcu is cortex-m3. if I have to get one of those jtag-like devices, will it work on cortex-m3. right?

your help is greatly appreciated. thanks in advance.

JTAG is used for debugging and programming. You can also use the boot loader for programming.

Cortex chips use the same JTAG interface.

Leon

The Stellaris Cortex-M3 chips also have the Serial Wire JTAG interface. I really have no idea how to use it, though. I can’t find any documentation on the hardware requirements. I’m assuming Crossworks doesn’t currently support it.

TheDirty:
The Stellaris Cortex-M3 chips also have the Serial Wire JTAG interface. I really have no idea how to use it, though. I can’t find any documentation on the hardware requirements. I’m assuming Crossworks doesn’t currently support it.

Whether SWD is supported or not in CrossWorks depends upon the JTAG interface in use. The J-Link supports SWD and we support that. The FTDI adapters (in general) do not, other than the Luminary and CodeRed adapters which have some special output stage.

paul_l_curtis:

TheDirty:
The Stellaris Cortex-M3 chips also have the Serial Wire JTAG interface. I really have no idea how to use it, though. I can’t find any documentation on the hardware requirements. I’m assuming Crossworks doesn’t currently support it.

Whether SWD is supported or not in CrossWorks depends upon the JTAG interface in use. The J-Link supports SWD and we support that. The FTDI adapters (in general) do not, other than the Luminary and CodeRed adapters which have some special output stage.

Thanks, Paul.

One thing that bugs me about these processors is making up a giant JTAG connector on each board. Even a 10pin JTAG header is big to me. I’ve been looking at some way to get the pincount down, or at least find a smaller connector that’s not expensive.

The 8bit uC’s I use have a single wire programming/debug interface. Moving from that to a 20pin connector has been a real hassle.

One technique that is sometimes used is to have the connector on an extension to the PCB that can be cut off following testing. Or, use pads and pogo pins

Leon

i 2nd stevech’s view on keil. I particularly like the visual representation of peripherals and the logic analyzer. great debugging tool.

wish hi-tech / eclipse were that good.

millwood:
i 2nd stevech’s view on keil. I particularly like the visual representation of peripherals and the logic analyzer. great debugging tool.

wish hi-tech / eclipse were that good.

If I wanted to be limited to less than 32k I would have stuck with 8bit MCU’s. I can see these being useful for production environments where you can pay the money, but 32k is a major limitation for development on an ARM chip, even for a hobbyist and full versions of these development environments are thousands of dollars.

CrossWorks is only $150 for a personal license.

Leon

TheDirty:
If I wanted to be limited to less than 32k I would have stuck with 8bit MCU’s.

there could be other reasons: speed, upward mobility, additional peripherals, costs, etc.

so far, I haven’t written a program with >8k code (.hex). so it will take me a while to breach that 32k barrier.

millwood:
there could be other reasons: speed, upward mobility, additional peripherals, costs, etc.

Speed, possibly, but there's some pretty fast 8bits and if you want speed without memory, there are other options.

Upward Mobility to what? You can’t go over 32k on the development platform you’ve chosen, without spending big $$'s.

There’s no peripherals on these chips that I don’t have on 8bit uC’s, the only benefit is using a lot of them at once, which brings us back to the memory problem.

Cost? What? ARM chips aren’t cheap.

millwood:
so far, I haven’t written a program with >8k code (.hex). so it will take me a while to breach that 32k barrier.

So, what happens when you do, and you've committed yourself to a development environment that you can't use unless you pay big $$'s for? SD Card FAT library, GLCD, RTOS, RF/Ethernet Stack... It doesn't take much to get over 32k. If I wasn't running firmware larger than 32k, I'd really question why I was using ARM chips at all.

IAR and Keil maybe fabulous, but they are a dead end for hobbyists unless you have $2.5k+ for a single seat license.

TheDirty:
Upward Mobility to what?

to more capable chips, if you DO indeed want to;

Cost? What? ARM chips aren’t cheap.

but they can be cheaper than 8-bit chips of comparable performance.

lm3s628 is $4.50/1 at digikey. that’s 60+mips chip, 8x10bit adc at 1msps, onboard temp sensor, 3 timers, 22 prioritized interrupt channels, tons of gpios, 2 uarts, rtc, mpu, etc.

the cheapest pic32 at digikey is $5+/1.

So, what happens when you do, and you’ve committed yourself to a development environment that you can’t use unless you pay big $$'s for? SD Card FAT library, GLCD, RTOS, RF/Ethernet Stack… It doesn’t take much to get over 32k.

I have committed myself to a development tool that costs me exactly $0 right now. and in the future, if I wanted to move up and don’t want fork over the cash, I can go other route, like GCC.

IAR and Keil maybe fabulous, but they are a dead end for hobbyists unless you have $2.5k+ for a single seat license.

they are a dead end for hobbyists who have to develop cost over 32k AND are unwilling / able to pay for the tools.

I would like to see when was you or another hobbyist actually developed a 32k or larger package.

I can see why they say you like to argue nonsensically.

Converting all your code to GCC is not trivial. Why would you start with a development tool that you can’t continue to use?

Your assertion that hobbyists using ARM chips do not go over 32k is frankly ridiculous and silly.

My embedded ethernet project is over 32k and I’ve just really started with this…

Code reusability is better with gcc as well. Your next project might be on say MIPS or Blackfin, and it’s nice to be able to repurpose generic code with minimum fuss. It’s also easier to use to unit test on an x86 system by mocking lower level drivers. Like a mock SD driver that returns sectors from a disk image.

+1 for GCC

It is a good compiler, it is available for many architectures ranging from desktop PCs to microcontrollers, and eases code portability.

When I moved form the AVR to the ARM it was easier because the compiler was the same.

On the ARM it takes a while getting used to it, but it’s definitely worth learning how to use it.

And based on some benchmark I made it also has very fast floating-point math on ARM.

And 32K code limit is a big problem for anybody doing serious microcontroller projects.

My last ARM project was an mp3 player and the code was 175KB, because it had:

  • 35KB of bitmap colour images stored to flash (even those alone would break the code limit!)

  • self-designed RTOS

  • FAT32 read/write library

  • part of the C and C++ standard library

  • many lines of code for GUI drawing, and application code