ARM7TDMI (STA8058)

Hi Folks~

I met a problem on config STA8058 chip (an arm7 based mcu).

Here comes the log message.

//================================================

Dennis@ /cygdrive/d/temp/openocd-0.2.0

$ ./openocd.exe -f tcl/interface/jlink.cfg -f tcl/target/str710.cfg

Open On-Chip Debugger 0.2.0 Release

$URL: http://svn.berlios.de/svnroot/repos/ope … rc/openocd

.c $

For bug reports, read http://svn.berlios.de/svnroot/repos/openocd/trunk/BUGS

10 kHz

Info : J-Link initialization started / target CPU reset initiated

Info : J-Link ARM V7 compiled Apr 1 2009 12:02:10

Info : JLink caps 0x39ff7bbf

Info : JLink hw version 70000

Info : JLink max mem block 8584

Info : Vref = 3.47 TCK = 1 TDI = 0 TDO = 1 TMS = 0 SRST = 1 TRST = 0

Info : J-Link JTAG Interface ready

Info : JTAG tap: str710.cpu tap/device found: 0x15323041 (mfg: 0x020, part: 0x53

23, ver: 0x1)

Error: JTAG tap: str710.cpu got: 0x15323041 (mfg: 0x020, part: 0x53

23, ver: 0x1)

Error: JTAG tap: str710.cpu expected 1 of 1: 0x3f0f0f0f (mfg: 0x787, part: 0xf0

f0, ver: 0x3)

Error: trying to validate configured JTAG chain anyway…

Error: Could not validate end of JTAG scan chain, IR mismatch, scan returned 0x0

  1. pos=4 expected 0x3 got 0

Warn : Could not validate JTAG chain, continuing anyway…

//==============================================

Since STR710 is an ARM7, I use its config file to config STA8058.

I already have checked the problem for several days.

Is it a config file setting issue?

Thanks,

Dennis

It seems to the multiple chain issue. Is there any one making it work with STR710? There are similar.

Dennis