Sorry if this is a duplicate: I thought I posted the question last week, but I don’t see it, so here goes again:
The Artemis integration guide shows a suggested circuit for the bootloader reset circuit. The issue is that the part values on the actual boards do not match the schematic for the DTR/BOOT circuit. Schematic shows R17 as “DNP” (do not populate?), but my board has a 10K. C21 on the schematic is 0.1uF cap, but the board has a 2.2uF cap. R15 is on the schematic as 220K, but the Sparkfun board has a 100K.
So which is right? What component values should be we using? I’m presuming we should use what the boards shipped with, but I figured I would ask.
I tried to upload an attachment of the Artemis schematic, but it is not working right now.