Artemis Firmware Uploader

I have the sparkfun redboard artemnis and I want to upload a bin file unto it using the artemis firmware uploader v2.0 but I keep getting errors. I have used different Baud Rate but still it did not work. I also tried to use the blink.bin file provided in the artemis firmware uploader folder to see if it works. but it also did not work. The error message I got is pasted below. This is on a windows machine.

Phase: Setup

Cleared startup blip

Phase: Bootload

Sending 8784 bytes in 5 frames

Error receiving packet

Unknown error

Sending frame #0, length: 0

Upload failed!

Also I want to be able to use the artemis firmware upload on a linux machine but when I double click the linux exe file provided in the linux folder, nothing happens. How can I upload flash my IMU connected to a linux machine without using the artemis firmware uploader, because it is not work for me.

Thank you in advance. :slight_smile:

Did the board previously work? Can you test some alternate cables?

I was not able to upload it with the linux exe file, so I used the arduino IDE to upload it. Thank you.

Linux can’t run EXE files, you’re stuck with Windows for those. :frowning:

It appears that the Artemis Uploader V3.1.0 “application is not supported” on macOS 15.5 based on the popup message shown after trying to launch it. Please note this is different than the “Apple could not verify” message and does not show up under Settings..Security with the option to “Open anyway”.

That’s a shame :-/

Can you downgrade or try some alternate method? (dual-boot, etc)

you could also consider to run the Python package as mentioned in the readme : GitHub - sparkfun/Artemis-Firmware-Upload-GUI: A cross-platform GUI for uploading new firmware to an Artemis based device.