The tracker can be powered from:
-
the USB-C interface
-
a LiPo battery (recharged via the USB-C interface)
-
an external solar panel or battery pack (6V maximum)
You can have the USB, LiPo and external cells connected simultaneously, it will do no harm.
If I connect the solar panel and Lipo for remote applications will the solar charge the battery and keep the system humming? I guess not due to the following additional instructions. I am not an electronics person but what is the design intent logic given the three power possibilities.
If you want to power the Global Tracker from a low current source, e.g. solar panels, the charge current can be reduced to 60mA by changing the Charge Current jumper link. The 60mA charge current is enough to offset the 9603N’s 39mA average current draw during receive, but bigger supercapacitors are needed to deliver the average current draw during a complete receive/transmit cycle. So, if you do change the charge current to 60mA, you will also need to solder additional 10 Farad supercapacitors on to the rear of the PCB using the solder pads provided.
What happens at night without solar. Would the 10 farads handle the duty cycle of receive and transmit cycle in general?
I am trying to deploy this into deep sea.
Given the current design, what is my best powering option to run the unit on solar with a backup LiPo battery?
Should I use a Solar Panel with Sunny Buddy and then feed power to the external cell power socket?