Hello everyone, i am currently using a As7265x sensor for spectroscopy analysis of beverages. I have placed the sensor attached to the surface of a glass first and then on the top of the glass looking down to the liquid. The two spectra are different. What do you recommend me to do for this kind of analysis?keeping the sensor attached to the surface?
Perform a similar analysis in an enclosed box, after disabling the 2 onboard LEDs from the AS7265x, again from below and above an empty mug, and treat that value differential as your baseline…then do the same for each liquid type and you’re very likely to be able to discern what is in the mug based on spectral readings
So i did an experiment in an enclosed box to avoid as much disturbance from external light as possible. My question is, this is the spectrum for a red wine, does the peaks means intensity of light reflected or absorbed? Since the sensor has mounted on it both emitters and receivers i suppose the peaks indicate the light that is reflected from the surface of the liquid and read back from the sensor.
That is correct