using USART in AT91SAM7S256…
receiver is not getting enabled…RXRDY remains 0.
using USART in AT91SAM7S256…
receiver is not getting enabled…RXRDY remains 0.
If transmitter works (i.e. clocks are ON) then ensure that:
USART pins are multiplexed correctly also for RX direction (disable PIO from controlling RX pin)
Multiplex RX I/O line to correct peripheral function (A/B)
Enable USART (transmitter and) receiver (US_CR)
I have AT91SAM7X256 development board and once above mentioned settings are correct then bidirectional data communication works with 115k2/8/N/1 settings i.e. once at least one character is received then RXRDY goes to 1 in US_CSR register.
done all d settings… bt still it doesn’t work…
can’t figure out d error…does anyone have a working code???