Hi All,
I want to implement a simple bootloader which communicates via ethernet only with a host (I won’t have any other access to the unit, so RS-232, USB is out of question). It would be a very simple code, to write the application into the flash, and execute it at startup.
I guess I won’t need any interrupts in the bootloader, but I’m sure I’ll have in the application.
I guess the bootloader before it starts the application should update the interrupt vector table, so when I jump to the application code, the application can use it.
Is anybody knows about any project where this is implemented?
Regards,
fpgakid