Have been lurking here for a while and think this forum is great, so I figured I would try my hand at asking for some help.
I am using an ATTINY2313, and have the ICP working fine using:
#include <avr/io.h>
#include <avr/interrupt.h>
#define READ(port,pin) (PIN ## port & (1<<pin))
#define INPUT(port,pin) DDR ## port &= ~(1<<pin)
#define OUTPUT(port,pin) DDR ## port |= (1<<pin)
#define CLEAR(port,pin) PORT ## port &= ~(1<<pin)
#define SET(port,pin) PORT ## port |= (1<<pin)
#define TOGGLE(port,pin) PORT ## port ^= (1<<pin)
volatile unsigned int pWidth;
volatile unsigned int pStart;
volatile unsigned int pStop;
int main (void)
{
INPUT(D,6); // Input Capture Pin set as input
SET(D,6); // Enable pull-up resistor
OUTPUT(B,0); // Declare PB0 as output
TCCR1B = (1<<CS11); // Set prescaler to 8
TCCR1B |= (1<<ICES1); // Input capture in rising edge
TIMSK = (1<<ICIE1); // Enable Input Capture interrupt
pWidth = 1500;
while(1)
{
sei();
if(pWidth <= 1470)
{
PORTB |= (1<<PB0);
}
else
{
PORTB &= ~(1<<PB0);
}
}
}
ISR(TIMER1_CAPT_vect)
{
PORTB ^= (1<<PB0);
pStop = ICR1;
if (TCCR1B & (1<<ICES1))
{
TCCR1B &= ~(1<<ICES1);
pStart = pStop;
}
else
{
TCCR1B |= (1<<ICES1);
pWidth = pStop - pStart;
}
}
I am wondering if I am searching for the holy grail by trying to incorporate a PWM output to an LED on the same timer? Or maybe I can not wrap my head around what needs to be done.
Is this even possible? If it is, what am I looking to do?
Is the code ok for what I am wanting or am I registers that are inhibiting the PWM out?
Ending result is to have one PWM being read on Timer0, one PWM being read on the ICP and to have the ICP PWM decide what duty cycle to be used for a PWM output.
Please show me the light. ![]()