AVR-ISP mkII

I found a module from Dontronics:

AVR-H128 ATMega128 Header Board

I wonder if this module is compatible Atmel AVR-ISP mkII and AVR Studio.

Thanks in advance.

Well the Dontronics [AVR-H128 Header board has a 10-pin ICSP header, and the ATmega128 is supported by [AVR Studio 4 (current version), and AVR-ISP mkII.

The AVR-ISP mk2 has a 6-pin (2x3) ISP cable, so you will need to a “fudge” adapter to remap the pins to connect from the 10-pin (2x5) ISP connector on the header board. There is even a [AVR ISP breakout board available from Spark Fun to make it easy to make such an adapter. So with that it should work fine.](SparkFun AVR Programming Adapter - BOB-08508 - SparkFun Electronics)](http://www.atmel.com/avrstudio/)](http://www.dontronics-shop.com/avr-h128-atmega128-header-board-with-stkxxx-compatible-10-pin-icsp-connector.html)