BC127 module mode source.

Hello community, good day.

I’ve been reviewing the BLC127 Bluetooth module, but I’m a bit confused about something. I hope you can help me. I understand that it works as a source and a sink, but in most places and uses, it’s called a sink. What I want to know is if, when using this module on my hardware, the application consists of taking audio generated in this case by analog signals through an ADC to i2s, and receiving these i2s signals through the module. I then put it in adversting mode so that some speakers can connect, and when doing so, I can send that audio via Bluetooth to the connected device. Basically, I want to send audio, not receive or those issues.
I’d like any information, and if there are any examples that I may have missed, thank you very much.

and to add and confirm this module is obsolete?

It is obsolete, we have a few examples available here Understanding the BC127 Bluetooth Module - SparkFun Learn