beaglebone timers not stopping on breakpoint

Im running on the beaglebone using libFTDI. I’ve enabled my timers to freeze in emulation mode however when I hit a breakpoint set either through gdb or directly through the openocd telnet interface the timers keep incrementing even though the code in the A8 has halted. This makes single stepping impossible as the timer continues to assert interrupts to the A8.

The TRM for the am335x is pretty vague but it says that when the PINSUSPENDN signal is asserted during emulation the timers will freeze. Any help on this would be appreciated.

Open On-Chip Debugger 0.7.0-dev-00079-g08ddb19 (2012-12-17-19:19)