The Goal:
I am trying to get the arduino (uno) to detect if the bluesmirf (silver) is connected or not by reading the status messages sent through serial (%CONNECT or %DISCONNECT)
What I’ve done:
Using the AT Command SO I have turned on “status messages” which sends a %CONNECT or %DISCONNECT string to the local serial port everytime the bluesmirf makes a connection or loses a connection.
The Problem:
I cannot figure out how to read those two different strings (%CONNECT/%DISCONNECT)
Side Notes:
I need the arduino to read either %CONNECT or %DISCONNECT and make a decision based on either finding.
Any help at all or a point in the correct direction would amazing. Thanks.
             
            
              
              
              
            
            
           
          
            
            
              Well since no one found anything I had to resolve this issue myself.
The answer:
In order to look for strings I had to use: find(string);
Here’s an example: ```
bluetooth.find(“%DISCONNECT”);
In that example find will look into the bluetooth for the string %DISCONNECT and if found will return true.
I have everything in a usable sketch on my website [http://www.carduino.vonini.com](http://www.carduino.vonini.com) (under arduino sketch) if anyone is interested in downloading the demo or seeing how I used it.
UPDATE:
Here is a sketch snippet from my website. It should give you a better idea of how I used find
void loop()
{
// LOCAL VARIABLES:
char c = bluetooth.find(“%CONNECT,30196692D7C0,0”);    // Read bluetooth and find given string
char d = bluetooth.find(“%DISCONNECT”);              // Read bluetooth and find %DISCONNECT string
if(c){                                                                  // Find %Connect String…
unlock();                                                             // Unlock the doors
}else if(d){                                                            // Find %Disconnect String…
lock();                                                               // Lock the doors
}else{                                                                  // If you can’t find either string then…
if(ul){                                                               // Check if Car is Unlocked…
if (dStatus()){                                                     // Now check to see if bluesmirf and phone are disconnected…
lock();                                                           // If it’s disconnected : Lock the doors
}                                                                   // BUT
}else{                                                                // If Car is Locked…
if (cStatus()){                                                     // Check to see if bluesmirf and phone are connected…
unlock();                                                         // If it’s connected : unlock the doors
}
}
}
if(r){                                                                  // Check to see if r(reconnect) is true…
reconnect();                                                          // If it is TRUE then reconnect
}
}//END: loop